Part Number: AM3356
Hello TI,
We are using the network boot function of the AM3356. We are using RGMII connection to the PHY, as with previous projects. We have a linux PC for the TFTP and BOOTP server. If we force the PC to be 100Mbps, the boot seems to work first time every time. If we let it use 1000 Mbps, it rarely works first time. We usually see no packets on wireshark until it restarts the boot process and it may take 5 minutes to complete the process. Eventually, it does boot at 1000 Mbps. Other than booting, there don’t seem to be any network problems at 1000Mbps. Have you heard of any similar issues?
The PHY_MODE[3:0] is set to 1110 = “advertise all capabilities except 1000Base-T half duplex” according to the datasheet. It always seems to work fine at 1000Mbps after booting.
Thanks,
Dan