Part Number: LINUXSDK-OMAPL138
Other Parts Discussed in Thread: DA8XX
Tool/software: Linux
Hi
I want to access spi from user space and kernel spcae.
It works fine from user space using /dev/spidev0.2.
I want also in some cases to acces this spi bus from kernel.
I understand that I have to use methods of spi.c such spidev.c does with spi_async() or spi_sync().
But it requires to supply the : struct spi_device *spi i.e. pointer to spi device opened and registered at board_omapl130-hawk.c
via da8xx_register_spi() which calls platform_device_register().
As I understand the device opened at init phase of the spidev_init() and spidev_probe() by linux launcher.
I see that spidev get it by user space ioctl call at via struct file *filp at : spidev_ioctl(struct file *filp, unsigned int cmd, unsigned long arg) by:
spidev = filp->private_data;
spin_lock_irq(&spidev->spi_lock);
spi = spi_dev_get(spidev->spi);
So, I need to know how to get this pointer ?
The sdk used is : ti-sdk-omapl138-lcdk-01.00.00
linux omap version is : 3.1.10-gf6fe6d8-dirty.
BR
Yehuda