This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3D DMA not working on 2nd call



I have to use a 3D DMA to extract Y data from an NTSC input stream on the DM6437.  I am using the basic EDMA driver calls found in edma3_lld_1_05_00\packages\ti\sdo\edma3\drv\src\edma3.c.  To extract the Y data points, I have acnt = 1, bcnt = 720 and ccnt = 480.  I use the following calls to set up the DMA channel:

EDMA3_DRV_requestChannel

EDMA3_DRV_setTransferParams

EDMA3_DRV_setSrcIndex

EDMA3_DRV_setDestIndex

EDMA3_DRV_setOptField

EDMA3_DRV_setSrcParams

EDMA3_DRV_setDestParams

I want to set off 1 event to trigger all ccnt transfers, so I have set up chaining by enabling the ITCCHEN bit.  I have the STATIC bit set to 0, as section 3.3 of the EDMA user's guide specifies.  I also have the TCINTEN bit set to notify the DSP when the entire transfer is complete.   The first event is kicked off by a call to EDMA3_DRV_enableTransfer.  I then use the EDMA3_DRV_waitAndClearTcc function to wait for completion to finish.

This works fine on the first call.  All the data is transferred and I can get past the EDMA3_DRV_waitAndClearTcc call.  However, the second time around no data is transferred and the DSP gets stuck in the EDMA3_DRV_waitAndClearTcc call.  The only way I can fix this is if I call EDMA3_DRV_freeChannel and go through the DMA channel initialization process again.  Does anyone know why I have to do this?  Shouldn't the next 3D transfer just work?

Thanks,

Jason