Part Number: AM3358
Tool/software: Linux
Hello,
We are developing an application for which we are using below component.
our "custom board" contains below components.
1. SOM Phy AM3358BZCZA100
2. Custom carrier board : All peripherals(Eth0,usb,sdd card slot )are placed by using "phyBOARD-WEGA-AM335x" as reference.
We are also having "phyBOARD-WEGA-AM335x" board.(this board SOM : phy AM3354BBZCZ80)
Now, We are using Images from "ftp://ftp.phytec.de/pub/Products/India/phyBOARD-WEGA-AM335x/Linux/PD14.0.0/images/".(Images_512MB)
using , these Images, we are able to boot "custom board" as well "phyBOARD-WEGA-AM335x".
we are getting console on UART.
Issue :
- With these pre built images, Ethernet on "phyBOARD-WEGA-AM335x" is working and we are able to ping connected host/router via ethernet.
- But, Ethernet on our custom board is not working.Link is not getting up with same images.
Hardware for custom board is same as "carrier board of phyBOARD-WEGA-AM335x"
Note :
- We have enabled DHCP in \etc\network\interfaces
Question :- Are we using correct images for our custom board??images for customboard and "phyBOARD-WEGA-AM335x" should be same as it is using phy-AM335x???if not, please suggest correct Images for custom one.
- Is there any need to change these prebuilt images?
- Is there any need to modify ethernet driver in given BSP??
If there is need to change driver or any kernel componant, can you suggest any link or document which will be useful to us??
attachment : we are attaching log for both custom as well phyBOARD-WEGA-AM335x.
barebox 2013.11.0 #1 Wed Jun 25 15:56:07 IST 2014
Board: Phytec phyBOARD-WEGA-AM335x
omap-hsmmc omap4-hsmmc0: registered as omap4-hsmmc0
mci0: registered disk0
probe buswidth
nand: ONFI param page 0 valid
nand: ONFI flash detected
nand: NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron MT29F4G08ABADAH4), 512MiB, page size: 2048, OOB size: 64
booting from MMC
barebox 2013.11.0 #2 Wed Jun 25 15:56:21 IST 2014
Board: Phytec phyBOARD-WEGA-AM335x
omap-hsmmc omap4-hsmmc0: registered as omap4-hsmmc0
mci0: registered disk0
cpsw cpsw0: detected phy mask 0x3
mdio_bus: miibus0: probed
eth0: got preset MAC address: 20:CD:39:FD:C4:2A
i2c-omap i2c-am33xx0: bus 0 rev0.11 at 100 kHz
probe buswidth
nand: ONFI param page 0 valid
nand: ONFI flash detected
nand: NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron MT29F4G08ABADAH4), 512MiB, page size: 2048, OOB size: 64
malloc space: 0x83ff4000 -> 0x87ff3fff (size 64 MiB)
Open /boot/barebox.env No such file or directory
no valid environment found on /boot/barebox.env. Using default environment
running /env/bin/init...
Hit m for menu or any other key to stop autoboot: 3 2 1 0
booting nand...
Image Name: Linux-3.2.0-PD13.0.0
OS: Linux
Architecture: ARM
Type: Kernel Image
Compression: uncompressed
Data Size: 3199592 Bytes = 3.1 MiB
Load Address: 80008000
Entry Point: 80008000
Loading OS U-Boot uImage '/dev/nand0.kernel.bb'
commandline: console=ttyO1,115200 ip=192.168.1.11:192.168.1.68:192.168.1.1:255.255.255.0::eth0: root=ubi0:root ubi.mtd=nand0.root,2048 rootfstype=ubifs da8xx_fb.panel_name=DVI_XGA mtdparts=omap2-nand.0:128k(nand0.xload),128k(nand0.xload_backup1),128k(nand0.xload_backup2),128k(nand0.xload_backup3),512k(nand0.barebox)ro,128k(nand0.bareboxenv),8M(nand0.kernel),-(nand0.root)
arch_number: 4144
[ 0.000000] Linux version 3.2.0-PD13.0.0 (bhaskar@pepl) (gcc version 4.7.3 20121106 (prerelease) (OSELAS.Toolchain-2012.12.1 linaro-4.7-2012.11) ) #1 Thu Feb 27 12:27:01 IST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: pcm051
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttyO1,115200 ip=192.168.1.11:192.168.1.68:192.168.1.1:255.255.255.0::eth0: root=ubi0:root ubi.mtd=nand0.root,2048 rootfstype=ubifs da8xx_fb.panel_name=DVI_XGA mtdparts=omap2-nand.0:128k(nand0.xload),128k(nand0.xload_backup1),128k(nand0.xload_backup2),128k(nand0.xload_backup3),512k(nand0.barebox)ro,128k(nand0.bareboxenv),8M(nand0.kernel),-(nand0.root)
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513168k/513168k available, 11120k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB)
[ 0.000000] .init : 0xc059d000 - 0xc05d8000 ( 236 kB)
[ 0.000000] .data : 0xc05d8000 - 0xc063aa60 ( 395 kB)
[ 0.000000] .bss : 0xc063aa84 - 0xc066c364 ( 199 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 25000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.056671] pid_max: default: 32768 minimum: 301
[ 0.056793] Security Framework initialized
[ 0.056915] Mount-cache hash table entries: 512
[ 0.057312] CPU: Testing write buffer coherency: ok
[ 0.058074] devtmpfs: initialized
[ 0.077728] omap_hwmod: pruss: failed to hardreset
[ 0.078918] print_constraints: dummy:
[ 0.079284] NET: Registered protocol family 16
[ 0.081665] OMAP GPIO hardware version 0.1
[ 0.084564] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.087738] omap_hsmmc.0: alias fck already exists
[ 0.089172] d_can.1: alias fck already exists
[ 0.090270] da8xx_lcdc.0: alias fck already exists
[ 0.091033] omap_i2c.1: alias fck already exists
[ 0.091369] davinci-mcasp.0: alias fck already exists
[ 0.091857] omap2_mcspi.1: alias fck already exists
[ 0.092132] omap2_mcspi.2: alias fck already exists
[ 0.092437] edma.0: alias fck already exists
[ 0.092437] edma.0: alias fck already exists
[ 0.092468] edma.0: alias fck already exists
[ 0.117034] bio: create slab <bio-0> at 0
[ 0.119262] SCSI subsystem initialized
[ 0.121093] usbcore: registered new interface driver usbfs
[ 0.121429] usbcore: registered new interface driver hub
[ 0.121643] usbcore: registered new device driver usb
[ 0.121795] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.122100] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.123382] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.124359] tps65910 1-002d: JTAGREVNUM 0x1
[ 0.127441] print_constraints: VRTC:
[ 0.128875] print_constraints: VIO: at 1500 mV
[ 0.131164] print_constraints: VDD1: 600 <--> 1500 mV at 1100 mV normal
[ 0.133392] print_constraints: VDD2: at 1100 mV
[ 0.134368] print_constraints: VDD3: 5000 mV
[ 0.135803] print_constraints: VDIG1: at 1800 mV
[ 0.137237] print_constraints: VDIG2: at 1800 mV
[ 0.138641] print_constraints: VPLL: at 1800 mV
[ 0.140045] print_constraints: VDAC: at 1800 mV
[ 0.141479] print_constraints: VAUX1: at 1800 mV
[ 0.142913] print_constraints: VAUX2: at 3300 mV
[ 0.144317] print_constraints: VAUX33: at 3300 mV
[ 0.145721] print_constraints: VMMC: at 3300 mV
[ 0.146057] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.148101] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.149536] cfg80211: Calling CRDA to update world regulatory domain
[ 0.150787] Switching to clocksource gp timer
[ 0.171112] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.171295] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.171630] MUSB0 controller's USBSS revision = 4ea20800
[ 0.171661] musb0: Enabled SW babble control
[ 0.172271] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using PIO, IRQ 18
[ 0.172454] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.172760] MUSB1 controller's USBSS revision = 4ea20800
[ 0.172760] musb1: Enabled SW babble control
[ 0.172912] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.172973] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.173156] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.173156] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.173187] usb usb1: Product: MUSB HDRC host driver
[ 0.173187] usb usb1: Manufacturer: Linux 3.2.0-PD13.0.0 musb-hcd
[ 0.173187] usb usb1: SerialNumber: musb-hdrc.1
[ 0.174133] hub 1-0:1.0: USB hub found
[ 0.174163] hub 1-0:1.0: 1 port detected
[ 0.174804] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using PIO, IRQ 19
[ 0.175262] NET: Registered protocol family 2
[ 0.175445] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.175781] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.176116] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.176330] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.176330] TCP reno registered
[ 0.176361] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.176361] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.176605] NET: Registered protocol family 1
[ 0.176910] RPC: Registered named UNIX socket transport module.
[ 0.176910] RPC: Registered udp transport module.
[ 0.176940] RPC: Registered tcp transport module.
[ 0.176940] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.177185] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.177398] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 0.177429] Registering NAND on CS0
[ 0.198272] VFS: Disk quotas dquot_6.5.2
[ 0.198333] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.198913] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.199249] msgmni has been set to 1002
[ 0.200073] io scheduler noop registered
[ 0.200073] io scheduler deadline registered
[ 0.200134] io scheduler cfq registered (default)
[ 0.202941] da8xx_lcdc da8xx_lcdc.0: GLCD: Found DVI_XGA panel
[ 0.233947] Console: switching to colour frame buffer device 128x48
[ 0.251953] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.253967] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.254455] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.960144] console [ttyO1] enabled
[ 0.964385] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.972045] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.979644] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.987274] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.006195] brd: module loaded
[ 1.015258] loop: module loaded
[ 1.018646] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.024932] i2c-core: driver [tsl2550] using legacy resume method
[ 1.031188] at24 1-0052: 4096 byte 24c32 EEPROM, writable, 32 bytes/write
[ 1.041198] omap2-nand driver initializing
[ 1.045745] ONFI flash detected
[ 1.049011] ONFI param page 0 valid
[ 1.052581] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron MT29F4G08ABADAH4)
[ 1.060729] 8 cmdlinepart partitions found on MTD device omap2-nand.0
[ 1.067260] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.072631] 0x000000000000-0x000000020000 : "nand0.xload"
[ 1.080078] 0x000000020000-0x000000040000 : "nand0.xload_backup1"
[ 1.087951] 0x000000040000-0x000000060000 : "nand0.xload_backup2"
[ 1.095733] 0x000000060000-0x000000080000 : "nand0.xload_backup3"
[ 1.103576] 0x000000080000-0x000000100000 : "nand0.barebox"
[ 1.111267] 0x000000100000-0x000000120000 : "nand0.bareboxenv"
[ 1.118774] 0x000000120000-0x000000920000 : "nand0.kernel"
[ 1.132354] 0x000000920000-0x000020000000 : "nand0.root"
[ 1.548858] OneNAND driver initializing
[ 1.553680] UBI: attaching mtd7 to ubi0
[ 1.557586] UBI: physical eraseblock size: 131072 bytes (128 KiB)
[ 1.563934] UBI: logical eraseblock size: 126976 bytes
[ 1.569427] UBI: smallest flash I/O unit: 2048
[ 1.574188] UBI: VID header offset: 2048 (aligned 2048)
[ 1.580261] UBI: data offset: 4096
[ 3.781158] UBI: max. sequence number: 4929
[ 3.799011] UBI: attached mtd7 to ubi0
[ 3.802917] UBI: MTD device name: "nand0.root"
[ 3.808380] UBI: MTD device size: 502 MiB
[ 3.813415] UBI: number of good PEBs: 4023
[ 3.818176] UBI: number of bad PEBs: 0
[ 3.822692] UBI: number of corrupted PEBs: 0
[ 3.827178] UBI: max. allowed volumes: 128
[ 3.831878] UBI: wear-leveling threshold: 4096
[ 3.836639] UBI: number of internal volumes: 1
[ 3.841125] UBI: number of user volumes: 1
[ 3.845642] UBI: available PEBs: 0
[ 3.850128] UBI: total number of reserved PEBs: 4023
[ 3.855163] UBI: number of PEBs reserved for bad PEB handling: 40
[ 3.861328] UBI: max/mean erase counter: 4/1
[ 3.865661] UBI: image sequence number: 36270686
[ 3.870544] UBI: background thread "ubi_bgt0d" started, PID 544
[ 3.877319] CAN device driver interface
[ 3.881225] CAN bus driver for Bosch D_CAN controller 1.0
[ 3.887664] d_can d_can.1: device registered (irq=55, irq_obj=56)
[ 3.941467] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 3.947723] davinci_mdio davinci_mdio.0: detected phy mask fffffffc
[ 3.955474] davinci_mdio.0: probed
[ 3.958923] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[ 3.967254] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver SMSC LAN8710/LAN8720
[ 3.975982] usbcore: registered new interface driver cdc_ether
[ 3.982116] usbcore: registered new interface driver cdc_subset
[ 3.988159] Initializing USB Mass Storage driver...
[ 3.993377] usbcore: registered new interface driver usb-storage
[ 3.999481] USB Mass Storage support registered.
[ 4.004577] usbcore: registered new interface driver usbserial
[ 4.010498] usbserial: USB Serial Driver core
[ 4.015594] mousedev: PS/2 mouse device common for all mice
[ 4.022369] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 4.030548] rtc-m41t80 1-0068: chip found, driver version 0.05
[ 4.038055] rtc-m41t80 1-0068: rtc core: registered rv4162c7 as rtc0
[ 4.046020] i2c /dev entries driver
[ 4.050384] lirc_dev: IR Remote Control driver registered, major 251
[ 4.056945] IR NEC protocol handler initialized
[ 4.061523] IR RC5(x) protocol handler initialized
[ 4.066375] IR RC6 protocol handler initialized
[ 4.070953] IR JVC protocol handler initialized
[ 4.075561] IR Sony protocol handler initialized
[ 4.080230] IR RC5 (streamzap) protocol handler initialized
[ 4.085876] IR MCE Keyboard/mouse protocol handler initialized
[ 4.091796] IR LIRC bridge handler initialized
[ 4.096313] Linux video capture interface: v2.00
[ 4.101348] usbcore: registered new interface driver uvcvideo
[ 4.107208] USB Video Class driver (1.1.1)
[ 4.113708] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 4.122192] cpuidle: using governor ladder
[ 4.126922] cpuidle: using governor menu
[ 4.136474] usbcore: registered new interface driver usbhid
[ 4.142181] usbhid: USB HID core driver
[ 4.148559] _regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
[ 4.156188] _regulator_get: 1-0018 supply DVDD not found, using dummy regulator
[ 4.163665] _regulator_get: 1-0018 supply AVDD not found, using dummy regulator
[ 4.171112] _regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
[ 4.182159] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
[ 4.190032] ALSA device list:
[ 4.193115] #0: PCM051
[ 4.195678] oprofile: hardware counters not available
[ 4.200775] oprofile: using timer interrupt.
[ 4.205139] nf_conntrack version 0.5.0 (8018 buckets, 32072 max)
[ 4.211914] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 4.217437] TCP cubic registered
[ 4.220733] NET: Registered protocol family 17
[ 4.225280] can: controller area network core (rev 20090105 abi 8)
[ 4.231628] NET: Registered protocol family 29
[ 4.236175] can: raw protocol (rev 20090105)
[ 4.240509] can: broadcast manager protocol (rev 20090105 t)
[ 4.246276] Registering the dns_resolver key type
[ 4.251129] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 4.258911] ThumbEE CPU extension supported.
[ 4.264099] Power Management for AM33XX family
[ 4.275451] Detected MACID=20:cd:39:fd:c4:2a
[ 4.281005] cpsw: Detected MACID = 20:cd:39:fd:c4:2c
[ 4.288726] rtc-m41t80 1-0068: setting system clock to 2155-12-31 23:17:09 UTC (1574614133)
[ 4.303985] net eth0: CPSW phy found : id is : 0x7c0f1
[ 4.386474] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 4.400421] mmc0: new high speed SDHC card at address aaaa
[ 4.406768] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 4.416961] mmcblk0: p1 p2
[ 5.332305] IP-Config: Complete:
[ 5.335601] device=eth0, addr=192.168.1.11, mask=255.255.255.0, gw=192.168.1.1,
[ 5.343322] host=192.168.1.11, domain=, nis-domain=(none),
[ 5.349365] bootserver=192.168.1.68, rootserver=192.168.1.68, rootpath=
[ 5.396057] UBIFS: recovery needed
[ 5.528442] UBIFS: recovery completed
[ 5.532257] UBIFS: mounted UBI device 0, volume 0, name "root"
[ 5.538208] UBIFS: file system size: 497491968 bytes (485832 KiB, 474 MiB, 3918 LEBs)
[ 5.546386] UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
[ 5.553894] UBIFS: media format: w4/r0 (latest is w4/r0)
[ 5.559844] UBIFS: default compressor: lzo
[ 5.564025] UBIFS: reserved for root: 0 bytes (0 KiB)
[ 5.570373] VFS: Mounted root (ubifs filesystem) on device 0:14.
[ 5.578125] devtmpfs: mounted
[ 5.582000] Freeing init memory: 236K
init started: BusyBox v1.20.2 (2014-04-18 12:21:11 IST)
starting pid 647, tty '/dev/console': '/etc/init.d/rcS'
mounting filesystems...done.
running rc.d services...
starting udev
creating static nodes
starting udevd...done
[ 5.923583] udevd[662]: starting version 182
waiting for devices...done
syslogd starting
klogd starting
crond starting
Starting system message bus: dbus.
hwclock: settimeofday: Invalid argument
starting sshd...done
Starting telnetd...
restoring mixer state.../usr/sbin/alsactl: parse:1655: Unable to open file '/usr/share/alsa/init/00main': No such file or directory
done
starting network interfaces...
RTNETLINK answers: File exists
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
[ 16.279296] net eth1: CPSW phy found : id is : 0x7c0f1
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
[ 25.370666] d_can d_can.1: can0: setting CAN BT = 0x209
[ 25.490386] tda998x 1-0034: Error -121 writing to cec:0xff
[ 25.500122] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.506408] dummy 1-0070: Error -121 reading from 0xa
[ 25.511749] dummy 1-0070: Error -121 writing to 0xa
[ 25.572357] dummy 1-0070: Error -121 reading from 0xa
[ 25.577667] dummy 1-0070: Error -121 writing to 0xa
[ 25.642272] dummy 1-0070: Error -121 reading from 0x1
[ 25.647583] dummy 1-0070: Error -121 writing to 0x1
[ 25.653045] dummy 1-0070: Error -121 reading from 0x1
[ 25.658355] dummy 1-0070: Error -121 writing to 0x1
[ 25.663787] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.669616] dummy 1-0070: Error -121 writing to 0x201
[ 25.675262] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.681091] dummy 1-0070: Error -121 writing to 0x27
[ 25.686614] dummy 1-0070: Error -121 reading from 0x0
[ 25.691925] dummy 1-0070: Error -121 reading from 0x2
[ 25.697082] found unsupported device: 0000
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//h_active: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//v_active: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//h_fporch: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//h_bporch: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//h_syncpw: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//v_fporch: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//v_bporch: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//h_syncpw: nonexistent directory
/etc/rc.d/S60dvi_startup: line 34: can't create /sys/module/tda998x_drv/drivers/i2c:tda998x/1-0034//v_syncpw: nonexistent directory
lighttpd: starting
lighttpd: done
/usr/sbin/pure-ftpd
pure-ftpd: starting pure-ftpd: /usr/sbin/pure-ftpd
/usr/sbin/pure-uploadscript
pure-ftpd: starting upload helper daemon...
done
starting inetd...done
Write Me
loading modules
[ 26.176391] gadget: using random self ethernet address
[ 26.181793] gadget: using random host ethernet address
[ 26.188232] usb0: MAC 86:f7:ae:22:52:a2
[ 26.192230] usb0: HOST MAC ba:15:bb:28:e5:d7
[ 26.196716] gadget: Ethernet Gadget, version: Memorial Day 2008
[ 26.202880] gadget: g_ether ready
[ 26.206390] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 26.211883] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 26.219665] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 26.226623] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 26.234008] usb usb2: Product: MUSB HDRC host driver
[ 26.239074] usb usb2: Manufacturer: Linux 3.2.0-PD13.0.0 musb-hcd
[ 26.245330] usb usb2: SerialNumber: musb-hdrc.0
[ 26.284515] hub 2-0:1.0: USB hub found
[ 26.288391] hub 2-0:1.0: 1 port detected
starting pid 792, tty '/dev/console': '/sbin/getty -L 115200 ttyO1 vt100'
____ _ ___ _______ _____ ____
| _ `| | | ` ` / /_ _| ____/ ___|
| |_) | |_| |` V / | | | _|| |
| __/| _ | | | | | | |__| |___
|_| |_| |_| |_| |_| |_____`____|
_ ____ ___ _ ____ ____ __ _______ ____
_ __ | |__ _ _| __ ) / _ ` / ` | _ `| _ ` ` ` / / ____/ ___|
| '_ `| '_ `| | | | _ `| | | |/ _ ` | |_) | | | |____` ` /` / /| _|| | _
| |_) | | | | |_| | |_) | |_| / ___ `| _ <| |_| |_____` V V / | |__| |_| |
| .__/|_| |_|`__, |____/ `___/_/ `_`_| `_`____/ `_/`_/ |_____`____|
|_| |___/
_ _ __ __ ______________
/ ` / ` | `/ |___ /___ / ___|_ __
/ _ ` _____ / _ ` | |`/| | |_ ` |_ `___ ` `/ /
/ ___ `_____/ ___ `| | | |___) |__) |__) > <
/_/ `_` /_/ `_`_| |_|____/____/____/_/`_`
OSELAS(R)-phyBOARD-WEGA-AM335x-PD13.0.0 / phyBOARD-WEGA-AM335x-PD13.0.0
ptxdist-2013.01.0/2014-04-18T12:24:54+0530
phyBOARD-WEGA-AM335x login: root
root@phyBOARD-WEGA-AM335x:~
root@phyBOARD-WEGA-AM335x:~
root@phyBOARD-WEGA-AM335x:~ ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
inet addr:127.42.23.180 Mask:255.255.255.0
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:55
eth0 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2A
UP BROADCAST ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
eth1 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2C
UP BROADCAST ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
usb0 Link encap:Ethernet HWaddr 86:F7:AE:22:52:A2
inet addr:192.168.56.4 Bcast:192.168.56.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@phyBOARD-WEGA-AM335x:~ [ 42.373229] PHY: 0:00 - Link is Up - 100/Full
root@phyBOARD-WEGA-AM335x:~ ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
inet addr:127.42.23.180 Mask:255.255.255.0
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:55
eth0 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2A
UP BROADCAST RUNNING ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:29 errors:0 dropped:10 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:7100 (6.9 KiB) TX bytes:0 (0.0 B)
eth1 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2C
UP BROADCAST ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
usb0 Link encap:Ethernet HWaddr 86:F7:AE:22:52:A2
inet addr:192.168.56.4 Bcast:192.168.56.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@phyBOARD-WEGA-AM335x:~ ifup eth0
udhcpc (v1.20.2) started
Sending discover...
Sending select for 192.168.0.107...
Lease of 192.168.0.107 obtained, lease time 7200
deleting routers
route: SIOCDELRT: No such process
adding dns 192.168.0.1
root@phyBOARD-WEGA-AM335x:~ ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
inet addr:127.42.23.180 Mask:255.255.255.0
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:55
eth0 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2A
inet addr:192.168.0.107 Bcast:192.168.0.255 Mask:255.255.255.0
UP BROADCAST RUNNING ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:211 errors:0 dropped:104 overruns:0 frame:0
TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:67847 (66.2 KiB) TX bytes:656 (656.0 B)
eth1 Link encap:Ethernet HWaddr 20:CD:39:FD:C4:2C
UP BROADCAST ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
usb0 Link encap:Ethernet HWaddr 86:F7:AE:22:52:A2
inet addr:192.168.56.4 Bcast:192.168.56.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@phyBOARD-WEGA-AM335x:~ ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Advertised pause frame use: Symmetric Receive-only
Advertised auto-negotiation: Yes
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 0
Transceiver: external
Auto-negotiation: on
Current message level: 0x00000000 (0)
Link detected: yes
root@phyBOARD-WEGA-AM335x:~ ping google.com
PING google.com (216.58.199.142): 56 data bytes
64 bytes from 216.58.199.142: seq=0 ttl=54 time=69.550 ms
64 bytes from 216.58.199.142: seq=1 ttl=54 time=127.808 ms
64 bytes from 216.58.199.142: seq=2 ttl=54 time=70.434 ms
64 bytes from 216.58.199.142: seq=3 ttl=54 time=67.993 ms
64 bytes from 216.58.199.142: seq=4 ttl=54 time=67.749 ms
64 bytes from 216.58.199.142: seq=5 ttl=54 time=68.207 ms
64 bytes from 216.58.199.142: seq=6 ttl=54 time=68.573 ms
--- google.com ping statistics ---
7 packets transmitted, 7 packets received, 0% packet loss
round-trip min/avg/max = 67.749/77.187/127.808 ms
root@phyBOARD-WEGA-AM335x:~ dmesg -c
[ 0.000000] Linux version 3.2.0-PD13.0.0 (bhaskar@pepl) (gcc version 4.7.3 20121106 (prerelease) (OSELAS.Toolchain-2012.12.1 linaro-4.7-2012.11) ) #1 Thu Feb 27 12:27:01 IST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: pcm051
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] On node 0 totalpages: 131072
[ 0.000000] free_area_init_node: node 0, pgdat c063173c, node_mem_map c066d000
[ 0.000000] Normal zone: 1024 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 130048 pages, LIFO batch:31
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttyO1,115200 ip=192.168.1.11:192.168.1.68:192.168.1.1:255.255.255.0::eth0: root=ubi0:root ubi.mtd=nand0.root,2048 rootfstype=ubifs da8xx_fb.panel_name=DVI_XGA mtdparts=omap2-nand.0:128k(nand0.xload),128k(nand0.xload_backup1),128k(nand0.xload_backup2),128k(nand0.xload_backup3),512k(nand0.barebox)ro,128k(nand0.bareboxenv),8M(nand0.kernel),-(nand0.root)
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513168k/513168k available, 11120k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB)
[ 0.000000] .init : 0xc059d000 - 0xc05d8000 ( 236 kB)
[ 0.000000] .data : 0xc05d8000 - 0xc063aa60 ( 395 kB)
[ 0.000000] .bss : 0xc063aa84 - 0xc066c364 ( 199 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 25000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.056671] pid_max: default: 32768 minimum: 301
[ 0.056793] Security Framework initialized
[ 0.056915] Mount-cache hash table entries: 512
[ 0.057312] CPU: Testing write buffer coherency: ok
[ 0.058074] devtmpfs: initialized
[ 0.077728] omap_hwmod: pruss: failed to hardreset
[ 0.078918] print_constraints: dummy:
[ 0.079284] NET: Registered protocol family 16
[ 0.081665] OMAP GPIO hardware version 0.1
[ 0.084564] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.087738] omap_hsmmc.0: alias fck already exists
[ 0.089172] d_can.1: alias fck already exists
[ 0.090270] da8xx_lcdc.0: alias fck already exists
[ 0.091033] omap_i2c.1: alias fck already exists
[ 0.091369] davinci-mcasp.0: alias fck already exists
[ 0.091857] omap2_mcspi.1: alias fck already exists
[ 0.092132] omap2_mcspi.2: alias fck already exists
[ 0.092437] edma.0: alias fck already exists
[ 0.092437] edma.0: alias fck already exists
[ 0.092468] edma.0: alias fck already exists
[ 0.117034] bio: create slab <bio-0> at 0
[ 0.119262] SCSI subsystem initialized
[ 0.121093] usbcore: registered new interface driver usbfs
[ 0.121429] usbcore: registered new interface driver hub
[ 0.121643] usbcore: registered new device driver usb
[ 0.121795] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.122100] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.123382] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.124359] tps65910 1-002d: JTAGREVNUM 0x1
[ 0.127441] print_constraints: VRTC:
[ 0.128875] print_constraints: VIO: at 1500 mV
[ 0.131164] print_constraints: VDD1: 600 <--> 1500 mV at 1100 mV normal
[ 0.133392] print_constraints: VDD2: at 1100 mV
[ 0.134368] print_constraints: VDD3: 5000 mV
[ 0.135803] print_constraints: VDIG1: at 1800 mV
[ 0.137237] print_constraints: VDIG2: at 1800 mV
[ 0.138641] print_constraints: VPLL: at 1800 mV
[ 0.140045] print_constraints: VDAC: at 1800 mV
[ 0.141479] print_constraints: VAUX1: at 1800 mV
[ 0.142913] print_constraints: VAUX2: at 3300 mV
[ 0.144317] print_constraints: VAUX33: at 3300 mV
[ 0.145721] print_constraints: VMMC: at 3300 mV
[ 0.146057] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.148101] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.149536] cfg80211: Calling CRDA to update world regulatory domain
[ 0.150787] Switching to clocksource gp timer
[ 0.171112] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.171295] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.171630] MUSB0 controller's USBSS revision = 4ea20800
[ 0.171661] musb0: Enabled SW babble control
[ 0.171691] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 0.171722] musb-hdrc: MHDRC RTL version 2.0
[ 0.171722] musb-hdrc: setup fifo_mode 4
[ 0.171752] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 0.171783] musb-hdrc.0: bulk split disabled
[ 0.171783] musb-hdrc.0: bulk combine disabled
[ 0.172271] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using PIO, IRQ 18
[ 0.172454] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.172760] MUSB1 controller's USBSS revision = 4ea20800
[ 0.172760] musb1: Enabled SW babble control
[ 0.172790] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 0.172821] musb-hdrc: MHDRC RTL version 2.0
[ 0.172821] musb-hdrc: setup fifo_mode 4
[ 0.172851] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 0.172851] musb-hdrc.1: bulk split disabled
[ 0.172882] musb-hdrc.1: bulk combine disabled
[ 0.172912] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.172973] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.173156] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.173156] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.173187] usb usb1: Product: MUSB HDRC host driver
[ 0.173187] usb usb1: Manufacturer: Linux 3.2.0-PD13.0.0 musb-hcd
[ 0.173187] usb usb1: SerialNumber: musb-hdrc.1
[ 0.174133] hub 1-0:1.0: USB hub found
[ 0.174163] hub 1-0:1.0: 1 port detected
[ 0.174804] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using PIO, IRQ 19
[ 0.175262] NET: Registered protocol family 2
[ 0.175445] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.175781] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.176116] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.176330] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.176330] TCP reno registered
[ 0.176361] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.176361] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.176605] NET: Registered protocol family 1
[ 0.176910] RPC: Registered named UNIX socket transport module.
[ 0.176910] RPC: Registered udp transport module.
[ 0.176940] RPC: Registered tcp transport module.
[ 0.176940] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.177185] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.177398] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 0.177429] Registering NAND on CS0
[ 0.198272] VFS: Disk quotas dquot_6.5.2
[ 0.198333] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.198913] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.199249] msgmni has been set to 1002
[ 0.200073] io scheduler noop registered
[ 0.200073] io scheduler deadline registered
[ 0.200134] io scheduler cfq registered (default)
[ 0.202941] da8xx_lcdc da8xx_lcdc.0: GLCD: Found DVI_XGA panel
[ 0.233947] Console: switching to colour frame buffer device 128x48
[ 0.251953] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.253967] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.254455] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.960144] console [ttyO1] enabled
[ 0.964385] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.972045] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.979644] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.987274] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.006195] brd: module loaded
[ 1.015258] loop: module loaded
[ 1.018646] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.024932] i2c-core: driver [tsl2550] using legacy resume method
[ 1.031188] at24 1-0052: 4096 byte 24c32 EEPROM, writable, 32 bytes/write
[ 1.041198] omap2-nand driver initializing
[ 1.045745] ONFI flash detected
[ 1.049011] ONFI param page 0 valid
[ 1.052581] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron MT29F4G08ABADAH4)
[ 1.060729] 8 cmdlinepart partitions found on MTD device omap2-nand.0
[ 1.067260] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.072631] 0x000000000000-0x000000020000 : "nand0.xload"
[ 1.080078] 0x000000020000-0x000000040000 : "nand0.xload_backup1"
[ 1.087951] 0x000000040000-0x000000060000 : "nand0.xload_backup2"
[ 1.095733] 0x000000060000-0x000000080000 : "nand0.xload_backup3"
[ 1.103576] 0x000000080000-0x000000100000 : "nand0.barebox"
[ 1.111267] 0x000000100000-0x000000120000 : "nand0.bareboxenv"
[ 1.118774] 0x000000120000-0x000000920000 : "nand0.kernel"
[ 1.132354] 0x000000920000-0x000020000000 : "nand0.root"
[ 1.548858] OneNAND driver initializing
[ 1.553680] UBI: attaching mtd7 to ubi0
[ 1.557586] UBI: physical eraseblock size: 131072 bytes (128 KiB)
[ 1.563934] UBI: logical eraseblock size: 126976 bytes
[ 1.569427] UBI: smallest flash I/O unit: 2048
[ 1.574188] UBI: VID header offset: 2048 (aligned 2048)
[ 1.580261] UBI: data offset: 4096
[ 3.781158] UBI: max. sequence number: 4929
[ 3.799011] UBI: attached mtd7 to ubi0
[ 3.802917] UBI: MTD device name: "nand0.root"
[ 3.808380] UBI: MTD device size: 502 MiB
[ 3.813415] UBI: number of good PEBs: 4023
[ 3.818176] UBI: number of bad PEBs: 0
[ 3.822692] UBI: number of corrupted PEBs: 0
[ 3.827178] UBI: max. allowed volumes: 128
[ 3.831878] UBI: wear-leveling threshold: 4096
[ 3.836639] UBI: number of internal volumes: 1
[ 3.841125] UBI: number of user volumes: 1
[ 3.845642] UBI: available PEBs: 0
[ 3.850128] UBI: total number of reserved PEBs: 4023
[ 3.855163] UBI: number of PEBs reserved for bad PEB handling: 40
[ 3.861328] UBI: max/mean erase counter: 4/1
[ 3.865661] UBI: image sequence number: 36270686
[ 3.870544] UBI: background thread "ubi_bgt0d" started, PID 544
[ 3.877319] CAN device driver interface
[ 3.881225] CAN bus driver for Bosch D_CAN controller 1.0
[ 3.887664] d_can d_can.1: device registered (irq=55, irq_obj=56)
[ 3.941467] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 3.947723] davinci_mdio davinci_mdio.0: detected phy mask fffffffc
[ 3.955474] davinci_mdio.0: probed
[ 3.958923] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[ 3.967254] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver SMSC LAN8710/LAN8720
[ 3.975982] usbcore: registered new interface driver cdc_ether
[ 3.982116] usbcore: registered new interface driver cdc_subset
[ 3.988159] Initializing USB Mass Storage driver...
[ 3.993377] usbcore: registered new interface driver usb-storage
[ 3.999481] USB Mass Storage support registered.
[ 4.004577] usbcore: registered new interface driver usbserial
[ 4.010498] usbserial: USB Serial Driver core
[ 4.015594] mousedev: PS/2 mouse device common for all mice
[ 4.022369] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 4.030548] rtc-m41t80 1-0068: chip found, driver version 0.05
[ 4.038055] rtc-m41t80 1-0068: rtc core: registered rv4162c7 as rtc0
[ 4.046020] i2c /dev entries driver
[ 4.050384] lirc_dev: IR Remote Control driver registered, major 251
[ 4.056945] IR NEC protocol handler initialized
[ 4.061523] IR RC5(x) protocol handler initialized
[ 4.066375] IR RC6 protocol handler initialized
[ 4.070953] IR JVC protocol handler initialized
[ 4.075561] IR Sony protocol handler initialized
[ 4.080230] IR RC5 (streamzap) protocol handler initialized
[ 4.085876] IR MCE Keyboard/mouse protocol handler initialized
[ 4.091796] IR LIRC bridge handler initialized
[ 4.096313] Linux video capture interface: v2.00
[ 4.101348] usbcore: registered new interface driver uvcvideo
[ 4.107208] USB Video Class driver (1.1.1)
[ 4.113708] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 4.122192] cpuidle: using governor ladder
[ 4.126922] cpuidle: using governor menu
[ 4.133758] Registered led device: peb_eval_01:green:led3
[ 4.136474] usbcore: registered new interface driver usbhid
[ 4.142181] usbhid: USB HID core driver
[ 4.148559] _regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
[ 4.156188] _regulator_get: 1-0018 supply DVDD not found, using dummy regulator
[ 4.163665] _regulator_get: 1-0018 supply AVDD not found, using dummy regulator
[ 4.171112] _regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
[ 4.182159] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
[ 4.190032] ALSA device list:
[ 4.193115] #0: PCM051
[ 4.195678] oprofile: hardware counters not available
[ 4.200775] oprofile: using timer interrupt.
[ 4.205139] nf_conntrack version 0.5.0 (8018 buckets, 32072 max)
[ 4.211914] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 4.217437] TCP cubic registered
[ 4.220733] NET: Registered protocol family 17
[ 4.225280] can: controller area network core (rev 20090105 abi 8)
[ 4.231628] NET: Registered protocol family 29
[ 4.236175] can: raw protocol (rev 20090105)
[ 4.240509] can: broadcast manager protocol (rev 20090105 t)
[ 4.246276] Registering the dns_resolver key type
[ 4.251129] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 4.258911] ThumbEE CPU extension supported.
[ 4.264099] Power Management for AM33XX family
[ 4.275451] Detected MACID=20:cd:39:fd:c4:2a
[ 4.281005] cpsw: Detected MACID = 20:cd:39:fd:c4:2c
[ 4.288726] rtc-m41t80 1-0068: setting system clock to 2155-12-31 23:17:09 UTC (1574614133)
[ 4.303985] net eth0: CPSW phy found : id is : 0x7c0f1
[ 4.386474] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 4.400421] mmc0: new high speed SDHC card at address aaaa
[ 4.406768] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 4.416961] mmcblk0: p1 p2
[ 5.332305] IP-Config: Complete:
[ 5.335601] device=eth0, addr=192.168.1.11, mask=255.255.255.0, gw=192.168.1.1,
[ 5.343322] host=192.168.1.11, domain=, nis-domain=(none),
[ 5.349365] bootserver=192.168.1.68, rootserver=192.168.1.68, rootpath=
[ 5.396057] UBIFS: recovery needed
[ 5.528442] UBIFS: recovery completed
[ 5.532257] UBIFS: mounted UBI device 0, volume 0, name "root"
[ 5.538208] UBIFS: file system size: 497491968 bytes (485832 KiB, 474 MiB, 3918 LEBs)
[ 5.546386] UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
[ 5.553894] UBIFS: media format: w4/r0 (latest is w4/r0)
[ 5.559844] UBIFS: default compressor: lzo
[ 5.564025] UBIFS: reserved for root: 0 bytes (0 KiB)
[ 5.570373] VFS: Mounted root (ubifs filesystem) on device 0:14.
[ 5.578125] devtmpfs: mounted
[ 5.582000] Freeing init memory: 236K
>[ 5.923583] udevd[662]: starting version 182
[ 16.279296] net eth1: CPSW phy found : id is : 0x7c0f1
[ 25.370666] d_can d_can.1: can0: setting CAN BT = 0x209
[ 25.490386] tda998x 1-0034: Error -121 writing to cec:0xff
[ 25.500122] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.506408] dummy 1-0070: Error -121 reading from 0xa
[ 25.511749] dummy 1-0070: Error -121 writing to 0xa
[ 25.572357] dummy 1-0070: Error -121 reading from 0xa
[ 25.577667] dummy 1-0070: Error -121 writing to 0xa
[ 25.642272] dummy 1-0070: Error -121 reading from 0x1
[ 25.647583] dummy 1-0070: Error -121 writing to 0x1
[ 25.653045] dummy 1-0070: Error -121 reading from 0x1
[ 25.658355] dummy 1-0070: Error -121 writing to 0x1
[ 25.663787] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.669616] dummy 1-0070: Error -121 writing to 0x201
[ 25.675262] dummy 1-0070: Error -121 writing to REG_CURPAGE
[ 25.681091] dummy 1-0070: Error -121 writing to 0x27
[ 25.686614] dummy 1-0070: Error -121 reading from 0x0
[ 25.691925] dummy 1-0070: Error -121 reading from 0x2
[ 25.697082] found unsupported device: 0000
[ 26.176391] gadget: using random self ethernet address
[ 26.181793] gadget: using random host ethernet address
[ 26.188232] usb0: MAC 86:f7:ae:22:52:a2
[ 26.192230] usb0: HOST MAC ba:15:bb:28:e5:d7
[ 26.196716] gadget: Ethernet Gadget, version: Memorial Day 2008
[ 26.202880] gadget: g_ether ready
[ 26.206390] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 26.211883] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 26.219665] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 26.226623] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 26.234008] usb usb2: Product: MUSB HDRC host driver
[ 26.239074] usb usb2: Manufacturer: Linux 3.2.0-PD13.0.0 musb-hcd
[ 26.245330] usb usb2: SerialNumber: musb-hdrc.0
[ 26.284515] hub 2-0:1.0: USB hub found
[ 26.288391] hub 2-0:1.0: 1 port detected
[ 42.373229] PHY: 0:00 - Link is Up - 100/Full
root@phyBOARD-WEGA-AM335x:~ lsusb
Bus 001 Device 001: ID 1d6b:0002
Bus 002 Device 001: ID 1d6b:0002
root@phyBOARD-WEGA-AM335x:~ root@phyBOARD-WEGA-AM335x:~ lsusbroot@phyBOARD-WEGA-AM335x:~ dmesg -croot@phyBOARD-WEGA-AM335x:~ ping google.comroot@phyBOARD-WEGA-AM335x:~ dmesg -cg
root@phyBOARD-WEGA-AM335x:~ [ 396.373260] PHY: 0:00 - Link is Down
root@phyBOARD-WEGA-AM335x:~ dmesg
[ 396.373260] PHY: 0:00 - Link is Down
root@phyBOARD-WEGA-AM335x:~
root@phyBOARD-WEGA-AM335x:~ ��