This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM57X: QtQuick.Controls version update

Part Number: PROCESSOR-SDK-AM57X

Tool/software: Linux

Hello, I've been working on a Qt/QML application with the AM57x EVM, using PSDK 4.0, and I've run into a small issue.  I have a UI element that is dependent on QtQuick.Controls version 2.2 (Popup, if it matters).  From what I can tell, this version of PSDK has QtQuick.Controls 2.0.  Can I update or install a new version of Controls?  Is this something that can be done through a new Yocto build?

Thank you in advance