Other Parts Discussed in Thread: SYSBIOS
I am using CCS v4.2 and trying to build SYS/BIOS project. I know about XGCONF editor and how you can edit CFG files with it. I am trying to set up a "periodic task" to run, like you could with the "PRD" option in TCF files used in DSP/BIOS version 5. Version 6 seems to be very different. There is a tab for "task" (under ti.sysbios.knl.Task), where I am assuming you specify the function to run "fxn" under "Create Args". Then there are options like arguments to the function and task priority, but I don't see anywhere where you can specify that the function should run "continuously" or give the interval at which it should execute. Is there a different way of doing it in SYS/BIOS? Maybe some combination of settings for clock, SWI, and task?