Other Parts Discussed in Thread: OMAP-L138
Hello
I want to use OMAP-L138 eXperimenter Kit with another devises. What are the connectors on the this board should be used, to connect to them? For example, connect to the ADC, through SPI. According to the document 1013125rev1_OMAP-L138_Baseboard_Schematic.pdf connectors interface SPI place on small contacts DF40C (labeling on the baseboard J13, J28, J29, etc.). So, to work with these interfaces i must interact through these small slot?