Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hi There,
I am using "VSDK_03_01_00_00" version of "VSDK" with TDA2XX SOC and able to build "VSDK" successfully for "Linux + Bios" platform . After that I have tried to execute below mentioned use case.
"NullSrc + Decode + Display". For executing this use case I have followed below mentioned steps.
1. I did some configuration for Display and Capture by using "Setting" option(S) (Here I have selected "HDMI 1080P60 for Capture" and "HDMI 1080P60 for Display").
2. Ran the "NullSrc + Decode + Display" use case and used the "H.264 " codec.
3. During the execution of use case I got "ASSERT (nullSrcLink_tsk.c|NullSrcLink_fillData|202)" on the console.
I read somewhere that "Linux+ Bios" doesn't have HDMI" support and I am not sure is this the case with Linux build.
Could someone please give clarification on this?.
Regards,
Anshul Jain.