Other Parts Discussed in Thread: CCSTUDIO
Hi, I am using the tms320cv5509a dsk . i have installed the code composer studio v4, i ran the diagnostic suite but it fails the POST, i am not able to understand whats going , i have checked with the power cables everything is good,
does any body have an answer, below is the output of the diagnostic suite
Habeeb
Driver Path :C:\CCSTUDIO_V3.1\DRIVERS
Driver Name :sdgo5510dsk.dvr
Board File Name :C:\CCSTUDIO_V3.1\DRIVERS\5509ADSKDiag.dat
Processor Name :cpu_0
Emulator Address :0x0540
==========================================================================
Starting diagnostic test suite.
--> Running USB diagnostics.
Can't connect to target.
*** Plug in power and USB cable.
*** Can't run if Code Composer or Diagnostic already running.
Result> USB diagnostic fail
Stopping diagnostic suite