This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

355 PLL power

Is there a document that describes the proper way to connect VDDA_PLL and VSSA_PLL pins? Should I connect VDDA_PLL to the  CVDD power plane and VSSA_PLL to the ground plane?

  • Gennadiy Kiryukhin said:
    Is there a document that describes the proper way to connect VDDA_PLL and VSSA_PLL pins? Should I connect VDDA_PLL to the  CVDD power plane and VSSA_PLL to the ground plane?

    The DM355 datasheet has example implementations of the Vdda_pll and Vssa_pll pins in sections 5.5.1 and 5.5.2. The PLL supplies would typically feed off of the Cvdd 1.3v power plane, though some extra capacitors and a ferrite bead are recommended.

    There is also an example implementation with the supplies combined on the EVM schematic, page 8.

  • I looked at the EVM schematic and it uses a separate ground where as Leopard Imaging 355 board has inductor in VDD line. I will follow the instructions in the datasheet.

    Thank you.