Hi,
My customer has the following questions:
For the TMS320C6455, is it possible to use four 16-bit DDR2 devices on the DDR2 bus?
We want to use a 32-bit bus and have the option of either using two 2Gb DDR2 devices, or four 1Gb devices to get 512 MByte of DDR2 SDRAM.
There is only one chip select, but with appropriate logic, can we decode the bank select signals and the chip select to access multiple devices for a given data bus?
Thanks,
Rick