Other Parts Discussed in Thread: OMAP3530, WL1271, OMAP3503
Hello,
I try to load the windows CE on Omap3530 but i get these result from Com Port.
Texas Instruments Windows CE SD X-Loader for EVM 3530
Built Sep 14 2010 at 16:55:43
Version 6.14.01
open ebootsd.nb0 file
Init HW: controller RST
SDHC: 1 bit mode
SDCARD: reqested speed 1000000, actual speed 1000000
Using 4 bit mode
SDHC: 4 bit mode
SDCARD: reqested speed 25000000, actual speed 24000000
BLSDCardDownload: cannot open file
SD boot failed to open file
HALT
Can you guy help me to solve it?
Thanks,
Behnam