On the OMAP-L137 device, pins F3 and H4 are designated as No Connect. If these pins are connected to ground, is there any harm to device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is a a note in the datasheet
Important Notice: On the original device pinout (marked "A" in the lower right corner of the package), pins USB0_VSSA33 (H4) and USB0_VSSA (F3) were connected to ground outside the package. For more robust ESD performance, the USB0 ground references are now connected inside the package on packages marked "B" and the package pins are unconnected. This change will require that any external filter circuits previously referenced to ground at these pins will need to reference the board ground instead.
It is fine if these pins are connected to ground. Inside the package they are now not connected to anything. No harm to the device.
OMAP-L137 Datasheet said:Important Notice: On the original device pinout (marked "A" in the lower right corner of the package), pins USB0_VSSA33 (H4) and USB0_VSSA (F3) were connected to ground outside the package. For more robust ESD performance, the USB0 ground references are now connected inside the package on packages marked "B" and the package pins are unconnected. This change will require that any external filter circuits previously referenced to ground at these pins will need to reference the board ground instead.
Is this also the case for OMAP-L138? The datasheet does not specify a pin number for USB0_VSSA33 and USB0_VSSA, but the EVM schematic shows these as pins M14 and N16, respectively, and connected to ground. The datasheet just lists those pins as NC.
So I guess I have two questions:
1) Do USB0_VSSA33 and USB0_VSSA have pin numbers?
2) If they do, does it matter how they're connected?
Thanks,
David