Below is a query sent by mail, that I am reposting to the forum....
Normal 0 false false false MicrosoftInternetExplorer4
Hi!
My faculty has an OMAP3530 EVM board and i am currently doing my thesis on this
board. I try to get the data returned from a usb webcam and modify them, then
display the image on the LCD screen. When i issue an open command to usb
webcam, it works, but it doesnt work with the read command, the byte return is
always -1. So what should i do?
By the way, i am connecting usb webcam on the usb host near UART 1/2, is that
ok? or i have to connect it to HUSB_OTG near the button.
Thanks
--
Lam Duong Minh Luan
Ho Chi Minh City - University of Technology
Faculty of Computer Science and Engineering
Phone number: 0947419836