This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 AMUTEIN input

If I use McASP0 serializer 0 as input, can the AMUTEIN input be used for stop receiving audio on this serializer or does this pin has no meaning when using only receive function?

  • The AMUTEIN does not actually stop the serializers, it simply passes through to the AMUTE signal so the McASP can work with other devices in the system that can generate a mute/error signal (see figure 33 of SPRUER1b), this being said if you want to stop receiving audio your driver would have to take in an event/interrupt and stop it in software (for example connecting the mute signal you would drive AMUTEIN with to a GPIO interrupt pin).