This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA746: Using 6AM.1.2: kernel edma memcpy

Part Number: DRA746


Question from customer:  Do you know if there are any benefits in enabling a couple edma-memcpy-channels in dts?
They've noticed this in the logs before:

[    0.565004] edma 43300000.edma: memcpy is disabled

And tracked it down to the related device tree bindings + this comment in their dts:
        /*
         * memcpy is disabled, can be enabled with:
         * ti,edma-memcpy-channels = <20 21>;
         * for example. Note that these channels need to be
         * masked in the xbar as well.
         */

Just wondering if it might lead to any performance gains or be worth looking into further.