Part Number: AM3352
Tool/software: Linux
Hi
I am working with a board based on the beagleBoneBlack using the latest SDK 04_01_00_06. Running a very small rootfs based on core-image-imnimal
I am trying to incorporate a sht3x temp/humdity sensor.
&i2c1 {
status = "okay";
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&i2c1_pins>;
sht@44 {
compatible = "sht3x";
reg = <0x44>;
};
};
Unfortunately the probe of this device fails unless I add printk debug text to the probe function
without debug:
[ 2.551089] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range [ 2.594213] input: tps65217_pwrbutton as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input1 [ 2.620112] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.659425] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.709542] sht3x: probe of 1-0044 failed with error -121 [ 2.715467] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
Whereas with some trivial debug in place (just a mark and a line number to see where the driver failed):
[ 2.584144] input: tps65217_pwrbutton as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input1 [ 2.610052] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.649363] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.670103] sht3 710 [ 2.699342] sht3 715 [ 2.701541] sht3 719 [ 2.703739] sht3 734 [ 2.714773] sht3 738 [ 2.716970] sht3 743 [ 2.728447] sht3 751 [ 2.731138] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz [ 2.745095] input: gpio_buttons@0 as /devices/platform/gpio_buttons@0/input/input2
I find that I have a working device:
root@elle-board:/sys/devices/platform/ocp/4802a000.i2c/i2c-1/1-0044/hwmon/hwmon0# ls device humidity1_input humidity1_min of_node temp1_alarm temp1_max_hyst uevent heater_enable humidity1_max humidity1_min_hyst power temp1_input temp1_min update_interval humidity1_alarm humidity1_max_hyst name subsystem temp1_max temp1_min_hyst
Relying on what I presume is timing effects of debug strings seems like a pretty poor way of getting something to work.
I would be grateful for any suggestions about how best to make this reliable?
Thanks for the help,
Richard