This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I hope to use the TI 2A Library in DVSDK environment.



I hope to use the TI 2A Library in DVSDK environment.

 

First of all, I succeed the capture RGB bare image. Also I convert YUV 4:2:0 and resize for encoder from the RGB image. Now I want to use TI 2A Library from the IPNC SDK package of APPRO RDK.

I find out the source code for example of TI 2A Library. I think the files are alg_aewb.c alg_aewb_control.c. and the IPNC_DM368-2.0.0 SDK include the ae_ti.c for Auto Exposure source code. But Auto White Balance is supported as binary library as “libti_awb.a”. The library have grovel variable AWB_TI_AWB for Auto White Balance analytic. But I cannot link the AWB_TI_AWB with ported source alg_aewb.c in dvsdk.

I tested the code in the directory in “dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/aewd”

Please help me !!!

 

I added the “-L. -lti_awb” on LD_FLAGS in Makefile

 

LD_FLAGS += -lpthread -lpng -ljpeg -lfreetype -lasound -L. -lti_awb

 

 

============================================================

Compiling alg_aewb.o from alg_aewb.c..

Compiling alg_aewb_control.o from alg_aewb_control.c..

alg_aewb_control.c:5: warning: ?ee_table??defined but not used

Compiling awb_calc_data.o from awb_calc_data.c..

Compiling TI_aewb_tables.o from TI_aewb_tables.c..

 

Linking aewd from ae_ti.o alg_aewb.o alg_aewb_control.o awb_calc_data.o TI_aewb_tables.o aewd_config/linker.cmd..

alg_aewb.o: In function `ALG_aewbCreate':

/home/ykjung/dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/aewd/alg_aewb.c:490: undefined reference to `AWB_TI_AWB'

alg_aewb.o: In function `TI2AFunc':

/home/ykjung/dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/aewd/alg_aewb.c:783: undefined reference to `RGB2RGB_stab'

/home/ykjung/dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/aewd/alg_aewb.c:797: undefined reference to `AWB_TI_AWB'

alg_aewb.o: In function `ALG_aewbDelete':

/home/ykjung/dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/aewd/alg_aewb.c:964: undefined reference to `AWB_TI_AWB'

collect2: ld returned 1 exit status

make: *** [aewd] Error 1