Part Number: DRA725
Other Parts Discussed in Thread: AB15
Tool/software: Linux
Hi,
now i use the battery to power the RTC module;
i add the driver that omap-rtc to kernel and i can measure the RTC_OSC_XI_CLKIN32 is 32.768KHz;
but i set date and reset the board,The date is not saved;
i set date : # date -s "2017-12-01 12:12:12"
# hwclock -w
V12/AB15/AB13 : Battery powered
If RTC can save time, how should the circuit be changed.
Regards,
Cesar