Part Number: TDA2EXEVM
Tool/software: Code Composer Studio
Hi,
I am trying set the input frequency(SYS_CLK1) 27 MHz for Timer 3 ,but it has not changed.For 27 MHz , I have made below setting on Evaluation board.
GPMC_AD8 (sysboot8) GPMC_D08 SW4.P1-OFF
GPMC_AD9 (sysboot9) GPMC_D09 SW4.P2 -ON
After this setting when we check the address 0x4A00 26C4 -CTRL_CORE_BOOTSTRAP in debug at that time we saw the pin 9 was set.
also set the 0x4AE0 6110-CM_CLKSEL_SYS for 27 MHZ. But frequency has not changed for 27 MHz.
according to the
32.2.4.2 System Clock Speed Selection
There are three crystal speeds available to be selected by means of sysboot[9:8], as described in
Table 32-7. User is responsible to set the correct value depending on the actual clock supplied to the
device.
Table 32-7. System Clock (SYS_CLK1) Speed Selection
sysboot[9:8] SYS_CLK1 Speed
0b00 Reserved
0b01 20 MHz
0b10 27 MHz
0b11 19.2 MHz
Please suggest ,how to configure timer 3 for 27 MHz.
Regards,
Kiran Vidhate