Part Number: TMS320DM368
Tool/software: Linux
Hi,
I have booted dm368 eval board with kernel from flash and file system using Network File system(NFS). I have the data being written into SDCard.
Without removing SDCard from the board, I want to read/write the files from SDCard to Desktop(Windows). There is miniUSB port available which can be connected to Desktop using MiniUSB to USB Cable.
what should be done so that SDCard contents can be seen on Desktop when Miniusb to USB cable is connected between LinuxBoard and Desktop PC?
Thanks in advance,
Regards
Neiki