This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Comparing image qualities of senor without aewb + 2A engine and senor with aewb + without 2A engine

Hi ,

I just want to comapare two cases.

1. (sensor without auto exposure + auto white balance features) + DM365 + H3A engine + 2A engine software 

2. (Senor with auto exposure + auto whitebalance) -like OV2715 omnivision) + DM365 + without using 2A engine software

How will be image qualities,when we compare these cases.

 

As I would like to migrate to DM368 which doesnot have H3A functions, this is really important.

(DM368 does not have H3A Engine ?  http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/60120/215860.aspx#215860  )

Please help me regarding this.

 

Thanks

tvs