Part Number: J6EVM5777
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
i am trying to run my DSP sysBios source code on the J6EVM Eval Board without the JTAG and CCS7.
In the last days, i did some research on the ti web site and the wiki about my project. I found only this site with some informations about the linux boot from my Jacinto 6 Evaluation Board. But this is not what i want to do.
My application is a SysBios implementation that runs very well on the DSP, but it runs only together with the JTAG and CCS7.
How can i flash the .out file to the DSP and how can i start/boot my programm with the ARM A15 from flash memory?
From my understanding, the ARM A15 is the master and all other controllers are slaves. That means the ARM A15 must enable the DSP and load my compiled application from flash into the DSP. Is this correct?
It's would be nice to have an example code with an documentation or start up guide.
best regards
Paul