Part Number: TMS320DM8148
Tool/software: Linux
Hello everyone,
I am having a problem with cross compiling Python using Code Sourcery toolchain. I am trying to compile it for TMS320DM8148 platform with Linux system installed (via EZSDK, kernel 2.6.37) in order to run OPBASM. Python sources compiling:
./configure -host=arm-none-linux-gnueabi CC=arm-none-linux-gnueabi-gcc RANLIB=arm-none-linux-gnueabi-ranlib STRIP=arm-none-linux-gnueabi-strip --build=arm-none-linux --disable-ipv6 ac_cv_file__dev_ptmx=no ac_cv_file__dev_ptc=no ac_cv_have_long_long_format=yes make CROSS_COMPILE=arm-none-linux-gnueabi- CROSS_COMPILE_TARGET=yes make install CROSS_COMPILE=arm-none-linux-gnueabi- CROSS_COMPILE_TARGET=yes prefix=~/Python-2.7.2/_install
Make command finishes successfully with following warning:
Python build finished, but the necessary bits to build these modules were not found:
_bsddb _curses _curses_panel
_sqlite3 _ssl _tkinter
bsddb185 bz2 dbm
dl gdbm imageop
linuxaudiodev ossaudiodev readline
sunaudiodev zlib
It seems like Python has been compiled for target machine, it can be run on it but I cannot start opbasm, it finishes with following errors:
root@dm814x-evm:~/nfs-share/opbasm# python opbasm.py meas_ctrl.hex Traceback (most recent call last): File "opbasm.py", line 32, in <module> import subprocess File "/home/root/Python/lib/python2.7/subprocess.py", line 72, in <module> import select ImportError: No module named select

I have also tried usin solution above, but the outcome is similar:
$ python opbasm.py meas_ctrl.hex
Traceback (most recent call last):
File "opbasm.py", line 41, in <module>
import opbasm.optimize as optimize
File "/home/pi/opbasm-master/opbasm/opbasm.py", line 41, in <module>
import opbasm.optimize as optimize
ImportError: No module named optimize
Could you help me find a solution for successful cross compilation Python on DM814?
Best regards,
Jacob