Part Number: PROCESSOR-SDK-AM335X
I used the rt818etv wireless network card test, and the SDK(ti-sdk-am335x-evm-07.00.00.00) integration driver was used, and the following errors were reported after repeated hot insertion.
so,I also tested it in the latest SDK(ti-processor-sdk-linux-rt-am335x-evm-04.01.00.06), tt will still cause the kernel to crash
What should I do?
==============================================================================================================================
root@am335x-evm:~# [ 429.291678] usb 1-1: USB disconnect, device number 10
[ 430.299007] ------------[ cut here ]------------
[ 430.303985] WARNING: CPU: 0 PID: 362 at drivers/usb/musb/musb_host.c:129 musb_h_tx_flush_fifo+0x60/0x9c [musb_hdrc]()
[ 430.315209] Could not flush host TX2 fifo: csr: 2403
[ 430.320459] Modules linked in: r8188eu(C) g_mass_storage usb_f_mass_storage libcomposite configfs musb_dsps musb_hdrc ti_am335x_adc industrialio musb_am335x
[ 430.335321] CPU: 0 PID: 362 Comm: khubd Tainted: G C 3.12.10-rt15-ti2013.12.01 #13
[ 430.344242] Backtrace:
[ 430.346865] [<c0016c9c>] (dump_backtrace+0x0/0x10c) from [<c0016e38>] (show_stack+0x18/0x1c)
[ 430.355785] r6:bf022cfb r5:00000009 r4:dd46bcc0 r3:00208040
[ 430.361836] [<c0016e20>] (show_stack+0x0/0x1c) from [<c052edbc>] (dump_stack+0x20/0x28)
[ 430.370322] [<c052ed9c>] (dump_stack+0x0/0x28) from [<c004108c>] (warn_slowpath_common+0x6c/0x8c)
[ 430.379713] [<c0041020>] (warn_slowpath_common+0x0/0x8c) from [<c0041150>] (warn_slowpath_fmt+0x38/0x40)
[ 430.389744] r8:c078099c r7:dd1dc404 r6:00000000 r5:00002403 r4:e093e522
[ 430.396911] [<c0041118>] (warn_slowpath_fmt+0x0/0x40) from [<bf01bd38>] (musb_h_tx_flush_fifo+0x60/0x9c [musb_hdrc])
[ 430.408043] r3:00000002 r2:bf022d18
[ 430.411886] [<bf01bcd8>] (musb_h_tx_flush_fifo+0x0/0x9c [musb_hdrc]) from [<bf01d3ac>] (musb_cleanup_urb+0x88/0xd8 [musb_hdrc])
[ 430.424018] r8:00000000 r7:dd6d0c80 r6:dd773554 r5:e093e520 r4:dd1dc404
[ 430.431195] [<bf01d324>] (musb_cleanup_urb+0x0/0xd8 [musb_hdrc]) from [<bf01d4f0>] (musb_urb_dequeue+0xf4/0x110 [musb_hdrc])
[ 430.443084] [<bf01d3fc>] (musb_urb_dequeue+0x0/0x110 [musb_hdrc]) from [<c03bf880>] (unlink1+0xb4/0xc4)
[ 430.453027] [<c03bf7cc>] (unlink1+0x0/0xc4) from [<c03c0cb8>] (usb_hcd_flush_endpoint+0x64/0xf0)
[ 430.462316] r7:dd0fe200 r6:dba0c27c r5:dba0c26c r4:dd6d0c80
[ 430.468354] [<c03c0c54>] (usb_hcd_flush_endpoint+0x0/0xf0) from [<c03c32a8>] (usb_disable_endpoint+0x68/0x80)
[ 430.478836] r7:00000000 r6:00000000 r5:dba0c26c r4:dd55e000
[ 430.484875] [<c03c3240>] (usb_disable_endpoint+0x0/0x80) from [<c03c3300>] (usb_disable_interface+0x40/0x50)
[ 430.495264] r6:dd55e000 r5:d9c49048 r4:00000002 r3:dba0c26c
[ 430.501302] [<c03c32c0>] (usb_disable_interface+0x0/0x50) from [<c03c5444>] (usb_unbind_interface+0x5c/0x168)
[ 430.511783] r8:bf0feff4 r7:00000000 r6:dd3c1000 r5:dd55e000 r4:dd3c1020
r3:00000000
[ 430.520138] [<c03c53e8>] (usb_unbind_interface+0x0/0x168) from [<c031aae0>] (__device_release_driver+0x84/0xcc)
[ 430.530815] [<c031aa5c>] (__device_release_driver+0x0/0xcc) from [<c031ab4c>] (device_release_driver+0x24/0x30)
[ 430.541499] r5:dd3c1020 r4:dd3c1054
[ 430.545327] [<c031ab28>] (device_release_driver+0x0/0x30) from [<c031a60c>] (bus_remove_device+0xe0/0xf0)
[ 430.555442] r5:dd430040 r4:dd3c1020
[ 430.559267] [<c031a52c>] (bus_remove_device+0x0/0xf0) from [<c0317ed0>] (device_del+0x110/0x174)
[ 430.568556] r6:dd55e068 r5:00000000 r4:dd3c1020 r3:00000002
[ 430.574601] [<c0317dc0>] (device_del+0x0/0x174) from [<c03c3394>] (usb_disable_device+0x84/0x19c)
[ 430.583982] r6:00000000 r5:00000000 r4:dd55e000 r3:0000000d
[ 430.590016] [<c03c3310>] (usb_disable_device+0x0/0x19c) from [<c03bacd0>] (usb_disconnect+0x88/0x148)
[ 430.599775] [<c03bac48>] (usb_disconnect+0x0/0x148) from [<c03bd43c>] (hub_thread+0x60c/0xea4)
[ 430.608895] [<c03bce30>] (hub_thread+0x0/0xea4) from [<c005a760>] (kthread+0xac/0xb8)
[ 430.617196] [<c005a6b4>] (kthread+0x0/0xb8) from [<c0013b98>] (ret_from_fork+0x14/0x3c)
[ 430.625682] r7:00000000 r6:00000000 r5:c005a6b4 r4:dd07de5c
[ 430.631724] ---[ end trace 0000000000000002 ]---
[ 431.644290] ------------[ cut here ]------------