Part Number: AM3351
Other Parts Discussed in Thread: TPS65910
I configured the AM3351ZCE with the PMIC TPS65910.
I measured all the power supplies, and it is correct.
I measured the clock and its correct.
I measured the clock1out, and it is correct too (24MHz).
And when i measured the serial signals does not show "C".
It is revision of the project that in the last revision the processor works fine.
Do you have some actions about what i need to do to bringup this processor?
Thanks.