Part Number: TMS320C5535
Hi,
I am working on a speech recognition project in my college. For this I used C5535EZDSP board and tried out the demo application, but accuracy is not that great with that (Suggest any improvements if possible). In document I saw the models can be generated, and training can be done using TIESR. I went ahead and followed to generate both SmallVocabulary and Normal Vocabulary(phones). Below are words I am using:
open door
close door
lock
unlock car
I recorded 8khz speech audio using audacity and segmented same audio for both SmallVocabulary and Normal (phones). I have used 22 recording for each word.
Then after successful training, I ran both Vocabulary in C5535 hardware. It works great, but one problem it shows random commands even when nothing is said.
I figured this is due to absence of filler model. I saw few posts in TI forum related to that and tried to follow. But I am not able to do it.
In normal vocabulary, the _fil garbage doesnt work properly. Please suggest what is wrong? What parameters I should change?
In SmallVocabulary, I have put fill as garbage. Here it works 70-80% good. But sometimes shows "lock" as random, without me saying anything. Then if I blow air, itll show fill. Please suggest what I need to do here to fix this? Any parameters need to be changed in this?
I am fresher student in this. So will be glad if some can mentor me in this step by step process.
Thanks,
Giridhar