This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: HS200 eMMC support

Part Number: AM5718

Tool/software: Linux

I want to use emmc HS200 mode.I find this function disabled in uboot code.

SDK 04.01.00.06

u-boot/drivers/mmc/omap_hsmmc.c

static int omap_hsmmc_platform_fixup(struct mmc *mmc)
{
    struct omap_hsmmc_data *priv = omap_hsmmc_get_data(mmc);
    struct mmc_config *cfg = omap_hsmmc_get_cfg(mmc);

    priv->version = NULL;

    if (platform_fixup_disable_uhs_mode()) {
        priv->version = "rev11";
        cfg->host_caps &= ~(MMC_MODE_HS200 | MMC_MODE_UHS_SDR104
                    | MMC_MODE_UHS_SDR50);
    }

    return 0;
}

cpu version 1.1 do not support? What about 2.0?