Part Number: AM3359
Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hello All,
I am using AM3358 from Sitara. I am using linux 3.2. I am having console on ttyO1 right now.
I have connected LCD to processor."fbtest" is running good and i can see number of Images.
Now i want to transfer console on LCD.
I have tried below...
1. change bootenv variable "console=/dev/fb0".
2. CONFIG_FRAMEBUFFER_CONSOLE=y
CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY=y
CONFIG_FRAMEBUFFER_CONSOLE_ROTATION=y
After this My boot in serial console stops at this line
"commandline: console=/dev/fb0 ip=192.168.1.11:192.168.1.68:192.168.1.1:255.255.)
arch_number: 4144"
But i can't see any line in LCD.Please suggest me if any other change is needed.