Other Parts Discussed in Thread: OMAP-L138, OMAP-L137, OMAPL138
Hi.
I have noticed that TI released the new OMAP-L138 processor with 375MHz clock. I am using LogicPD development kits with 300MHz processors. Is it possible to overclock those processors to 375MHz? If is understood correctly from the PLL datasheet it is impossible to achieve 375MHz clock with 24MHz crystal which is used in the kit and I must replace the crystal to 25MHz for example, am I right?
Another question is regarding uBoot and Linux. Are there available precompiled binaries for 375MHz clock?
Thanks, Alexey.