This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM368: TMS320DM368 (DVSDK running on it) interface with CC3100

Part Number: TMS320DM368


Hello Everyone,

Right now we are working on CC3100  and  TMS320DM368 for our media applications

we have Leopard board 368 on which we are running one of the SDK's (DVSDK) ,how to add one of the user application say use a GPIO as I/O for blinking LED or use an UART to interface with the TMS320DM368

We have procured CC3100 booster wifi module.

we need to use CC3100 with TMS320DM368 via UART for one of our media application.

We have gone through the following wiki

CC3100 UART Host Interface - Texas Instruments Wiki

processors.wiki.ti.com

and interfaced with Tiva series launchpad and ran one of the example program and saw the UARTdata in the serial hyper terminal.

But now we need to replace the host as TMS320DM368 on which TI DVSDK will be running.

How to add UART configuration (user application) to the TI DVSDK ? any Example or application note available?

Thank you ,

Regards,

Sanath Rai