This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4372: HS device cannot boot

Part Number: AM4372

Tool/software: Linux

We now design our SOM4372 core-board, use AM4372HS CPU(secure-boot P/N), but could not bootup,

the detail steps as following:
1) we use TI release SDK is
ti-processor-sdk-linux-am437x-hs-evm-04.01.00.06-Linux-x86-Install.bin & ti-processor-sdk-secdev-am437x-hs-01.05.00.06.tar.gz
2.) Base on
<Processor_SDK_Secdev_Build_Install_Guide> to make up the image file:  boot -> MLO & u-boot.img, the log imformation as attached file<log.txt>
Question: We want to c8535.log.txtonfirm whether need another TI key for boot up? If do not need , what should we do next?