Part Number: AM3352
Tool/software: Linux
Hi,
I am re-opening this issue beacuse the answer can't be found:
Because a Memory "DDR3 MT41K256M16HA-125:E" phases out, it has been to replaceed. From Micron's side the Memory Type "MT41K256M16TW-107:P" has been proposed as replacement.
But the CAS Latency of "MT41K256M16TW-107:P" is not matched with TI am3352 supported latency. The CAS Latency of "MT41K256M16TW-107:P" is 13 and Max CAS Latency supported by AM3352 is 11.
Attached Figure from P.932@TI AM3352 TRM:
Attached Figure is from MICRON DDR3L SDRAM MT41K256M16TW-107:P SPEC
Is there any resolution or workaround about this?
Br,
Josko