Part Number: AM3352
Tool/software: Linux
Hi :
I am strange that in the lastest TRM ,
5-0 BASEADDRESS R/W 0h Chip-select base address.
CSi base address where i = 0 to 3 (16 Mbytes minimum granularity).
Bits 5 to 0 correspond to A29, A28, A27, A26, A25, and A24.
it said that CSi base where i=0 to 3 ?
Is that mean gpmc_cs4 gpmc_cs5 gpmc_cs6 can not be used as chip select pin and no memory space for it ?
Or it is a mistake in TRM
Best regards
wangl