This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSLCDK6748: CCS V3.3 using XDS100V3 emulator

Part Number: TMDSLCDK6748
Other Parts Discussed in Thread: OMAP-L138

Hi everyone,

I have a board LCDK_OMAP_L138 ,i want to test it with CCS v3.3 for with TI XDS100V3 .All i did is installed ccsv3.3 ,and it created two  icons on my desktop  CCS Studio V303 & Setup CCS studio.

I just opened the Setup CCS studio to import the board LCDK_6748/OMAP_L138. but LCDK is not there listed in c6000 family.

I tried looking for drivers  on Spectrum Digital Website but didnt get any.

Please see the image below 

I just need to know if i can work with ccsv3.3 for LCDK/OMAP (6748) boards,where to get the drivers for same.So that it will get listed in the above field.

ThanK You