Hi,
Some simple questions regarding the installation of these libraries for the C5505 etc..
- If the C55XCSL-LOWPOWER 2.01 is allready installed in the CCS install directory, can the C55XCSL-LOWPOWER 2.10 be installed on top without causing any conflicts ? Should they be kept sepparate in sepparate install directories ?
- Is there a default windows environment variable that sets the CSL installation paths (as I cannot seeme to find one like for the DSP/BIOS and cgt tools) ?
- I notice that upon installing C55XCSL-LOWPOWER 2.10 (the latest CSL) there is no /lib directory installed and no cslVC5505L.lib (for 5505/5504 large and small memory models) are provided with this version, not unlike version 2.01 which had these provided ? What is the story there ?
- in the build directory, compiling and creating a cslVC5505_Lib.lib file will essentially provide the same functions as with the cslVC5505L.lib provided in version 2.01 for instance ?? Just wondering why the version 2.01 had these libraries provided, but version 2.10 does not ?
regards, Mike