This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8127: DM8127: Using only 16 bit DDR3 instead of 32bit DDR3

Genius 9385 points

Part Number: TMS320DM8127

My customer is planning on using only 16-bit DDR3 interface. The 16 bit mode is supported according to the TRM by setting narrow mode field in SDRCR. However, there is not information about hardware configuration for 16 bit interface support.

Is there any recommendation on unused pin termination for DDR3? I assume lower numbered data lines are used ie D0:D15 are connected to the memory device? How do unused DQS and DQM lines need to be terminated?

Thanks!