This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8168: TMS320DM8168

Part Number: TMS320DM8168

Hello Friends,

I am facing the issue of USB hang in the case of USB mouse ( All manufactured) at 4kV contact type ESD . In the case of Pandrive it is working fine. I have used ESD protection diode at differential line which has limit upto 8 kV. Routing is done as per texas high interface reference document. I can not understand that issue come only for USB mouse and not for pendrive.

MPU:- TMS320DM8168

Please suggest me if any one have idea related to this issue.

Thanks,

Ronak