Part Number: AM3517
We have a shipping product based on the Logic PD AM3517 SOM module (SOMAM3517-10-1780RJCR) which contains an AM3517 processor. Their datasheet describes as a commercial temperature rated device. (70 degrees C max).
How do do you characterize that ambient with respect to air temperature at what distance and with what sort of flow? Does this assume any airflow? Is there a MAX "case temperature" spec for the processor that I might reference so that I might take a clear attached thermocouple measurement to clear up my thermal environment questions?
I ask because I see both network and USB issues as temperatures rise. (though are still below the 70c limit....the way I measure it) These also get far worst with lower voltage......so I wonder if my thermal environment might actually be higher than I think.