This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437_demo compile error.

I tiried to build DM6437_demo.pjt

but there was some error as follow.

 

 

Load error is apeared.

I search all cmd file section information....but there was not 0x42000000 memory map...

I connected this memory address to NOR flash memory.

 

and I am wondering about there is many waning after build completing.

Is there any problem?

thanks

 

 . 

Best regards Pansu Jang.

>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 266: warning:
               (.text:_H264MPVDEC_TI_mb_header) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 267: warning:
               (.text:_H264MPVDEC_TI_decode_nmb_P) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 268: warning:
               (.text:_H264MPVDEC_TI_decode_mvd_refidx) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 269: warning:
               (.text:_H264MPVDEC_TI_residual_block_cavld) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 270: warning:
               (.text:_H264MPVDEC_TI_set_available_mb) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 271: warning:
               (.text:_H264MPVDEC_TI_bbox_calculations) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 272: warning:
               (.text:_H264MPVDEC_TI_bbox_calc_1bb) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 273: warning:
               (.text:_H264MPVDEC_TI_aso_read_coeff) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 274: warning:
               (.text:_H264MPVDEC_TI_get_edgestr_intermb) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 275: warning:
               (.text:_H264MPVDEC_TI_aso_calc_mvp) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 276: warning:
               (.text:_H264MPVDEC_TI_more_rbsp_data) not found

,,,,,,,,,,,,,,,,,,,,,,,,,

,,,,,,,,,,,,,,,,,,,,,,,,,,,

>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 498: warning:
               (.text:dmaInit:_H264MPVDEC_TI_dmaInit) not found
>> C:\\dvsdk_1_01_00_15\\dm6437_demo_1_30_00\\xdcconfig\\linker.cmd, line 499: warning:
               (.text:dmaGetChannelCnt:_H264MPVDEC_TI_dmaGetChannelCnt) not
               found
>> warning: creating output section H264VDEC_TI_dSect1 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_dSect2 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect1 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect2 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect3 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect4 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect5 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect6 without SECTIONS
            specification
>> warning: creating output section H264VDEC_TI_cSect7 without SECTIONS
            specification

Build Complete,
  0 Errors, 204 Warnings, 0 Remarks.