Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3356
Tool/software: Code Composer Studio
I use AM3356-ZCZ and would like to use K17pin and K16pin as QEP mode as encoder counter.
But it is necessary to detect present High/Low status of the pins as GPI mode, too.
When I input 3.3V into 16pin, the voltage of K16 becomes 2.2V.
And GPI_INPUT_REGISER is kept "0".
I think that even if K16 is QEP mode, GPI register detects whether High or Low.
What should I check?