Other Parts Discussed in Thread: SYSBIOS
Tool/software: Linux
In thread "AM335x ICEv2 issue with IGH EtherCAT Master for Linux" there is mentioned a running example with the IgH-EtherCAT master with CIA402. Where can I access that example?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Linux
In thread "AM335x ICEv2 issue with IGH EtherCAT Master for Linux" there is mentioned a running example with the IgH-EtherCAT master with CIA402. Where can I access that example?
I tried also the latest ethercat slave app and MLO for the AM355x ICE r2.1 with the IgH Master.
But the device will not change to OP. There is an error during activating OP:
EtherCAT ERROR 0-0: Timeout while setting state OP.
Can i get a running example for the ICE with IgH master?
[26885.290384] EtherCAT DEBUG 0: IDLE -> ORPHANED.
[26885.290386] EtherCAT DEBUG 0: Stopping master thread.
[26885.290743] EtherCAT DEBUG 0: Master IDLE thread exiting...
[26885.290747] EtherCAT 0: Master thread exited.
[26885.309981] EtherCAT 0: Link state of ecm0 changed to DOWN.
[26885.460990] EtherCAT 0: Releasing main device 00:1B:21:0F:18:C3.
[26885.465740] EtherCAT: Master module cleaned up.
[26887.647723] EtherCAT: Master driver 1.5.2 2eff7c993a63
[26887.647779] EtherCAT: 1 master waiting for devices.
[26887.661373] ec_e1000e: EtherCAT-capable Intel(R) PRO/1000 Network Driver - 1.9.5-k-EtherCAT
[26887.661375] ec_e1000e: Copyright(c) 1999 - 2012 Intel Corporation.
[26887.661389] ec_e1000e 0000:03:00.0: Disabling ASPM L1
[26887.661521] ec_e1000e 0000:03:00.0: (unregistered net_device): Interrupt Throttling Rate (ints/sec) set to dynamic conservative mode
[26887.661590] ec_e1000e 0000:03:00.0: irq 44 for MSI/MSI-X
[26887.833187] EtherCAT: Accepting 00:1B:21:0F:18:C3 as main device for master 0.
[26887.977057] EtherCAT 0: Starting EtherCAT-IDLE thread.
[26887.977073] ec_e1000e 0000:03:00.0: (unregistered net_device): (PCI Express:2.5GT/s:Width x1) 00:1b:21:0f:18:c3
[26887.977075] ec_e1000e 0000:03:00.0: (unregistered net_device): Intel(R) PRO/1000 Network Connection
[26887.977164] ec_e1000e 0000:03:00.0: (unregistered net_device): MAC: 1, PHY: 4, PBA No: D50854-003
[26889.832490] ec_e1000e 0000:03:00.0: (unregistered net_device): 10/100 speed: disabling TSO
[26889.832494] EtherCAT 0: Link state of ecm0 changed to UP.
[26889.833597] EtherCAT 0: 1 slave(s) responding on main device.
[26889.833599] EtherCAT 0: Slave states on main device: PREOP.
[26889.833714] EtherCAT 0: Scanning bus.
[26889.848033] EtherCAT 0: Bus scanning completed in 14 ms.
[26889.848035] EtherCAT 0: Using slave 0 as DC reference clock.
[26889.848036] EtherCAT ERROR 0: Failed to calculate bus topology.
[26893.528390] EtherCAT 0: Master debug level set to 1.
[26901.712328] EtherCAT: Requesting master 0...
[26901.712330] EtherCAT DEBUG 0: IDLE -> OPERATION.
[26901.712332] EtherCAT: Successfully requested master 0.
[26901.712334] EtherCAT DEBUG 0: ecrt_master_create_domain(master = 0xffff8800d7892000)
[26901.712335] EtherCAT DEBUG 0: Created domain 0.
[26901.712338] EtherCAT DEBUG 0: ecrt_master_slave_config(master = 0xffff8800d7892000, alias = 0, position = 0, vendor_id = 0x0000088f, product_code = 0x4d490002)
[26901.712340] EtherCAT DEBUG 0: Creating slave configuration for 0:0, 0x0000088F/0x4D490002.
[26901.712343] EtherCAT DEBUG 0 0:0: Slave 0 has no matching vendor ID (0xE000059D) for configuration (0x0000088F).
[26901.712352] EtherCAT DEBUG 0 0:0: ecrt_slave_config_create_sdo_request_err(sc = 0xffff8800d7988000, index = 0x1C12, subindex = 0x00, size = 1)
[26901.712364] EtherCAT DEBUG 0 0:0: ecrt_slave_config_sync_manager(sc = 0xffff8800d7988000, sync_index = 0, dir = 1, watchdog_mode = 2)
[26901.712366] EtherCAT DEBUG 0 0:0: ecrt_slave_config_sync_manager(sc = 0xffff8800d7988000, sync_index = 1, dir = 2, watchdog_mode = 2)
[26901.712368] EtherCAT DEBUG 0 0:0: ecrt_slave_config_sync_manager(sc = 0xffff8800d7988000, sync_index = 2, dir = 1, watchdog_mode = 1)
[26901.712371] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_assign_clear(sc = 0xffff8800d7988000, sync_index = 2)
[26901.712373] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_assign_add(sc = 0xffff8800d7988000, sync_index = 2, pdo_index = 0x1601)
[26901.712376] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_mapping_clear(sc = 0xffff8800d7988000, pdo_index = 0x1601)
[26901.712379] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_mapping_add(sc = 0xffff8800d7988000, pdo_index = 0x1601, entry_index = 0x7010, entry_subindex = 0x00, entry_bit_length = 32)
[26901.712382] EtherCAT DEBUG 0 0:0: ecrt_slave_config_sync_manager(sc = 0xffff8800d7988000, sync_index = 3, dir = 2, watchdog_mode = 2)
[26901.712384] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_assign_clear(sc = 0xffff8800d7988000, sync_index = 3)
[26901.712386] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_assign_add(sc = 0xffff8800d7988000, sync_index = 3, pdo_index = 0x1A00)
[26901.712388] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_mapping_clear(sc = 0xffff8800d7988000, pdo_index = 0x1A00)
[26901.712390] EtherCAT DEBUG 0 0:0: ecrt_slave_config_pdo_mapping_add(sc = 0xffff8800d7988000, pdo_index = 0x1A00, entry_index = 0x6000, entry_subindex = 0x00, entry_bit_length = 32)
[26901.712393] EtherCAT DEBUG 0: ecrt_master_slave_config(master = 0xffff8800d7892000, alias = 0, position = 0, vendor_id = 0x0000088f, product_code = 0x4d490002)
[26901.712396] EtherCAT DEBUG 0 0:0: ecrt_slave_config_reg_pdo_entry(sc = 0xffff8800d7988000, index = 0x6000, subindex = 0x00, domain = 0xffff8800d5fcecc0, bit_position = 0xffff8800d70d7e24)
[26901.712399] EtherCAT DEBUG 0: Domain 0: Added 4 bytes, total 4.
[26901.712400] EtherCAT DEBUG 0: ecrt_master_slave_config(master = 0xffff8800d7892000, alias = 0, position = 0, vendor_id = 0x0000088f, product_code = 0x4d490002)
[26901.712403] EtherCAT DEBUG 0 0:0: ecrt_slave_config_reg_pdo_entry(sc = 0xffff8800d7988000, index = 0x7010, subindex = 0x00, domain = 0xffff8800d5fcecc0, bit_position = 0xffff8800d70d7e24)
[26901.712405] EtherCAT DEBUG 0: Domain 0: Added 4 bytes, total 8.
[26901.712408] EtherCAT DEBUG 0 0:0: ecrt_slave_config_dc(sc = 0xffff8800d7988000, assign_activate = 0x0300, sync0_cycle = 500000, sync0_shift = 4400000, sync1_cycle = 0, sync1_shift = 0
[26901.712419] EtherCAT DEBUG 0: ecrt_domain_external_memory(domain = 0xffff8800d5fcecc0, mem = 0xffffc90005779000)
[26901.712421] EtherCAT DEBUG 0: ecrt_master_callbacks(master = 0xffff8800d7892000, send_cb = 0xffffffffa0479750, receive_cb = 0xffffffffa0477d20, cb_data = 0xffff8800d7892000)
[26901.712423] EtherCAT DEBUG 0: ecrt_master_activate(master = 0xffff8800d7892000)
[26901.712426] EtherCAT DEBUG 0: Adding datagram pair with expected WC 3.
[26901.712427] EtherCAT 0: Domain0: Logical address 0x00000000, 8 byte, expected working counter 3.
[26901.712429] EtherCAT 0: Datagram domain0-0-main: Logical offset 0x00000000, 8 byte, type LRW.
[26901.712430] EtherCAT DEBUG 0: Stopping master thread.
[26901.712436] EtherCAT DEBUG 0: Master IDLE thread exiting...
[26901.712441] EtherCAT 0: Master thread exited.
[26901.712443] EtherCAT DEBUG 0: FSM datagram is ffff8800d7892678.
[26901.712444] EtherCAT 0: Starting EtherCAT-OP thread.
[26901.712458] EtherCAT DEBUG 0: Operation thread running with fsm interval = 1000 us, max data size=11250
[26901.712461] EtherCAT DEBUG 0: mmap()
[26901.712463] EtherCAT DEBUG 0: Vma fault, virtual_address = 00007f1beab1f000, offset = 0, page = ffffea0000a79a48
[26901.713466] EtherCAT DEBUG 0: Configuration changed.
[26901.713467] EtherCAT DEBUG 0-0: Checking system time offset.
[26901.714472] EtherCAT DEBUG 0-0: DC 64 bit system time offset calculation: system_time=26927911363880 (corrected with 1000000), app_time=26927912043907, diff=680027
[26901.714475] EtherCAT DEBUG 0-0: Not touching time offset.
[26901.715479] EtherCAT DEBUG 0: Requesting OP...
[26901.717486] EtherCAT DEBUG 0-0: Changing state from PREOP to OP.
[26901.717487] EtherCAT DEBUG 0-0: Configuring...
[26901.719493] EtherCAT DEBUG 0-0: Now in INIT.
[26901.719494] EtherCAT DEBUG 0-0: Clearing FMMU configurations...
[26901.720498] EtherCAT DEBUG 0-0: Clearing sync manager configurations...
[26901.721502] EtherCAT DEBUG 0-0: Clearing DC assignment...
[26901.722505] EtherCAT DEBUG 0-0: Configuring mailbox sync managers...
[26901.722507] EtherCAT DEBUG 0-0: SM0: Addr 0x1000, Size 128, Ctrl 0x26, En 1
[26901.722509] EtherCAT DEBUG 0-0: SM1: Addr 0x1080, Size 128, Ctrl 0x22, En 1
[26901.725522] EtherCAT DEBUG 0-0: Now in PREOP.
[26901.725525] EtherCAT DEBUG 0-0: SM2: Addr 0x1100, Size 4, Ctrl 0x64, En 1
[26901.725527] EtherCAT DEBUG 0-0: SM3: Addr 0x1400, Size 4, Ctrl 0x20, En 1
[26901.728545] EtherCAT DEBUG 0-0: Now in SAFEOP.
[26906.725393] EtherCAT ERROR 0-0: Timeout while setting state OP.
[26906.726400] EtherCAT 0: Slave states on main device: SAFEOP.
[26910.967714] EtherCAT 0: Slave states on main device: SAFEOP + ERROR.
[26910.968719] EtherCAT DEBUG 0-0: SAFEOP -> SAFEOP + ERROR.
Hi David
I used that prebuild sd card image 1.0.5.0.
this is the output on uart:
StarterWare Boot Loader
BOARDInit status [0x0]
SoC : [AM335X]
Core : [A8]
Board Detected : [ICE Ver 2]
Base Board Revision : [UNKNOWN]
Daughter Card Revision: [UNKNOWN]
GPIO Instance number: 0
Pin number: 18
MMC/SD Card Detect Pin Not Used on Hardware
Copying application image from MMC/SD card to RAM
Jumping to StarterWare Application...
Version - EtherCAT Slave 1.0.5.0
Board name : A335_ICE
Board Revision : 2.1AEtherCAT Device
SYS/BIOS EtherCAT Demo application3.3.0Rotary switch state : 0
Matthias
Hi Matthias
Regretfully, it is necessary to build the full application enable the CIA_402 mode.
Translating Lyu Frank steps in the previous post to the current Processor SDK & PRU-ICSS EtherCAT architecture
Follow the steps in http://processors.wiki.ti.com/index.php/PRU_ICSS_EtherCAT#Building_full_feature_EtherCAT_Slave_Application
Modify the macro value of TIESC_APPLICATION from 1 to 0, CiA402_DEVICE from 0 to 1.
Then addition to modifying the TI_ESC application it is necessary to also modify the IGH master (main.c) code.
Step 1: The boards have to be flashed with the EEPROM of cia402.
Step 2: The correct PDO entries have to be copied to the main.c file of IGH master.
sudo ethercat cstruct -> is the command to get the PDO entries.
The result of the above command will be different for TIESC_APPLICATION and CiA402_DEVICE
Step 3: The function call, "ecrt_slave_config_reg_pdo_entry" in main.c file of IGH master has to be modified with the obtained addresses from the step 2 command.
Step 4: Compile the master code.
make
David
Hi David,
these steps I had tried but with no success. next step should be compiling the Building_full_feature_EtherCAT_Slave_Application... when i have the SSC code.
I found kast week some other really curious behavior:
Hence, there was a miracle. TwinCAT does some magic config. So after TwinCAT does something, IGH can read/write the objects 0x6000/0x7010. Writing 0x7010 will only work correctly with type uint32. The propagated type octet_string delivers come strange data.