This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Custom board boot issue

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hi all,

I am working on a project where we are using a custom board that is based on the BeagleBone Black to boot. The custom board has removed most of the peripherals but left the most main hardware on the board. I am trying to flash the eMMC via a SD card but have been unable to get the board up and running. The board will go through the boot process and then keep restarting instead of launching the kernel. Attached is the serial output. Any help or insight on how to fix this would be appreciated!

BBB-blank-debian-8-9-LXQT-2GB-ARMHF-2017-11-02-2GB.txt