Part Number: DRA746
For MMC DMA to work correctly, is it required to configure IRQ cross bar (or) DMA cross bar is sufficient?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA746
For MMC DMA to work correctly, is it required to configure IRQ cross bar (or) DMA cross bar is sufficient?
Hi Jeba,
I work on Vision SDK package.
I have pinged a GLSDK expert who will help you on this.
Regards,
Rishabh
devicetree.rarHi RK,
we are using SDIO Card.
Please find the attached dts, dtsi file. also attached the configuration file that we are using.
Kindly check are we missing anything?
Please provide details for the below also
1. What should be the Source address for our Transfer configuration (P set)
2. Which event number we should use for the MMC1_DREQ_RX
3. we are using DMA cross bar 62 is this correct?
Thanks and Regards,
Sangeetha
Hi RK,
Kindly provide the details.
Please provide details for the below also
1. What should be the Source address for our Transfer configuration (P set)
2. Which event number we should use for the MMC1_DREQ_RX
3. we are using DMA cross bar 62 is this correct?
Do you have the chance to see the attachment as you requested. kindly provide your feedback.
Thanks and Regards,
Sangeetha
Hi Sangeeta,
Yes, I have been through the files and I have a few questions.
I'm not quite clear on what are you trying to do here.
Regards,
RK
sdio_irq_issue_1.xlsxHi RK,
Please find the below details and the attachment for better understanding,
We are trying to connect an external FPGA to the SD slot via SDIO interface.
For this we have written a driver code in polling mode to read the data, this is working fine and we are able to read the data properly.
We want to update this code to use EDMA, but this is not working for us. Please find the attached sheet “sdio_irq_issue_1.xlsx” for more details.
1. Without edma_start(i.e.Manual trigger) EDMA call back is not occurring. ( We expect the call back to be event triggered by EDMA_DREQ_61) Please educate us to configure Event triggering instead of current manual triggering.
2 We cannot set the MPU_IRQ_83 (MMC1_RX) line. Is our configuration procedure correct?
Kindly inform us are we missing anything in the configuration.
Hi RK,
We were not able to use the TI Frame work as such. since we are using customer specific FPGA which has a different command flow than the default kernel.
please find the below steps we have checked
1. With TI framework, 'omap_hsmmc_probe' is success and can able to register IRQ properly. (Filename: drivers/mmc/host/omap_hsmmc.c)
2. While trying 'mmc_rescan_try_freq()' in drivers/mmc/core/core.c, sdio_reset() call is failing. It is because of the stuck at mmc_io_rw_direct_host() call inside sdio_reset(). As we are using customer specific FPGA board, we cannot use the CMD52 given in the mmc_io_rw_direct_host() andso stuck occurs.
3. If we ignore sdio_reset() call, it is again failing in mmc_send_io_op_cond() API while calling mmc_attach_sdio(). mmc_send_io_op_cond() is trying to send CMD5 which is not supported by our FPGA. So we have excluded TI's flow and hardcoded MMC1 with our own commands to setup FPGA board (ie) PAD mux, clock configuration, init procedure, bus power configuration, sequence of commands (Reset, SDR mode set & READ MULTIPLE BLOCK commands) to FPGA.
4. After this procedure, we are able to see interrupts for data read. If I put OMAP_HSMMC_READ(host->base, DATA) inside interrupt handler I can get the correct read value(We aware of data read procedure should not be inside interrupt handler. But for the initial check we tried like this). So here we can confirm that data is read by polling method. Next we are trying to read the data by DMA.
5. We understood that DMA is already configured in omap_hsmmc_probe() and can get tx_chan and rx_chan.
6. Now the question is, what API we need to use to get data from DMA. What is the source and destination address? In omap_hsmmc_request() API, we can see the omap_hsmmc_start_dma_transfer() call. But we cannot figure out when this omap_hsmmc_request() getting called. If we call it manually, this call is not succeeded.
We are not receiving any DMA callback function also.
Kindly provide your inputs, how we can proceed further.
Thanks and Regards,
Sangeetha
Hi RK,
We have checked as per your suggestion with the compatibility flag.
Now we are able to transmit commands in finite transfer type and read data through this driver.
Default all the commands are transmitted as finite transfer type, if we change that to infinite transfer type there is no command complete.
after this there is no response.
Kindly suggest.
CC: Sangeetha
Dear RK,
Thanks for the help.
We are sending CMD0 and CMD18 for our FPGA board.
For Finite transfer,
1) we have initialized sg buffer with dma size(current size is 20480 bytes).
2) Set block length as 512
3) Set block count as dma_size/block length (ie) 20480/512 = 40 blocks
4) Set stop opcode too in mmc_request structure
Result:
i) Got one dma callback after CMD18 CC completes.
ii) Got one TC interrupt after 20480 bytes transferred.
iii) Read values are ok.
For InFinite transfer,
We have disabled BCE in sdio_hsmmc_start_command() and the remaining flow is same as finite transfer steps (1) to (4). [We understand that setting block count will not affect if we disable BCE bit]
Result:
i) Got one dma callback after CMD18 CC completes.
ii) Not getting TC interrupt. Because of this driver code got stuck after this line.
As this is infinite transfer, 'req_in_progress' value will be 1 in dma callback API. So mmc_request_done() will not be called. But why we are not getting TC interrupt?
For finite transfer also, we are expecting TC interrupt after every block length (512)bytes transferred. But we are getting it only after full size is transferred. Response is same for EDMA as well as SDMA. ITCINTEN is not set in edma code (drivers/dma/edma.c). It hangs the system when I'm trying to enable it. Is this is the root cause for the infinite transfer issue? If so, Kindly let us know how to fix it.
Regards,
Rajeswari S
Dear RK,
In addition to previous message, we have tried stream oriented transfer instead of block transfer. STR bit is set in CON register. For this also, we got the same response as like infinite block transfer. (ie) Got one dma callback after CMD18 CC completes, NOT getting TC interrupt and got stuck.
Anything have we missed out seriously while going for continuous data?
Thanks,
Rajeswari S
Dear RK,
Thanks for the reply.
We are not preferring 'Stop at Block Gap' feature as it will cause real time data miss out. Anyway we will give a try.
Regarding infinite transfer, we already sent CMD12(STOP). Still we are not getting TC, so stuck occurs. Please find the used code below:
/* Send CMD 18 (READ_MULTIPLE_BLOCK) */
memset(ptr->buffer, 0, size);
sg_init_one(&sg, ptr->buffer, size);
mrq.cmd = &cmd;
mrq.data = &data;
mrq.stop = &stop;
mrq.cmd->opcode = MMC_READ_MULTIPLE_BLOCK;
mrq.cmd->arg = 0x4809C220;
mrq.cmd->flags = MMC_RSP_R1 | MMC_CMD_ADTC;
mrq.data->blksz = blocklen; /* blocklen = 512 */
mrq.data->blocks = (size / blocklen); /* size = 20480, it does not matter as we set infinite transfer */
mrq.data->flags = MMC_DATA_READ;
mrq.data->sg = &sg;
mrq.data->sg_len = sg_len;
mrq.stop->opcode = MMC_STOP_TRANSMISSION;
mrq.stop->arg = 0;
mrq.stop->flags = MMC_RSP_R1B | MMC_CMD_AC;
mmc_wait_for_req(host->mmc, &mrq);
Any suggestion on this RK?
Regards,
Rajeswari S
Hi Rajeswari,
The following assignment is wrong
mrq.cmd->arg = 0x4809C220;
This should be the argument for the CMD18 which is the address of the first data block that needs to be read form the card not MMCHS_DATA.
It should be a valid block address between 0x0 and the max number of sectors (blocks) -1.
Regards,
RK
Hi RK,
Thank you very much for your support.
Still we are facing some issues in configuring the SDIO with our FPGA. Currently we have put this task on hold.
We will ask for any clarifications if needed in future.
Thanks and Regards,
Sangeetha