Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352
I'm having an issue with certain custom boards with the AM3352 processor halting (I think) shortly after booting up. When I say halted, I mean all the peripherals stop working, the screen stops updating, and I cannot even connect over the JTAG header to the processor. When trying to connect through JTAG using CCS, I just get "Unable to halt device. Reset the device, and retry the operation".
On Windows CE 7, I start up the OS, I see the desktop, and usually the start menu graphic has not been loaded (just a blue box in the corner, the same color as the desktop background). I can attach screenshots if that will help.
I realize TI does not support Windows CE, but I see this as more of a processor-specific issue that I'm having. I have run both Windows CE 7 and TI's Arago Linux distro (the bug is easier to replicate on Windows) and have seen this halting issue in both OSs and I'm wondering what kinds of situations can cause the processor to behave this way.
Any assistance would be appreciated,
Kevin