This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: DDR3 finding problem

Part Number: TMS320C6678

Hi I want to build my custom board with TMS320C6678 core. the EVM used "K4B2G1646E-BCH9" as DDR3 with maximum rate 1333M but I need use industerial part of it which will be "K4B2G1646E-BIH9" but I undrestood these days this part is unreachable and SAMSUNGcompany don't build anymore. Do you have any recommended part with the following specification? Please help me. Thanks.

Density : >= 2Gb 

Voltage : 1.5V

temp :   Industerial

Package : 96FBGA

Data Bus: 16 bit

DDRCLK : 66MHz