Following the readme.txt in C:\Program Files\Texas Instruments\pspdrivers_01_30_00_06\packages\ti\pspiom\cslr\evm6748\examples\spi I tried to load and build this example. But...I get the error, "could not open source file "ti/pspiom/cslr/soc_C6748.h""
In the project Includes is the directory, "C:\Program Files\Texas Instruments\pspdrivers_01_30_00_06\packages\ti". Ah ha! The "/ti/" is surperfluous. Upon closer examination the include path "${EXT_ROOT__spi_example}/../../../../.." does not have enough dot-dots. Added "/..", now it builds.
But...that is not the question. Another include path is "${C6000_CSL_CG_ROOT}/include". C6000_CSL_CG_ROOT is not set. The path becomes "/include".
This raises the first question, why not? Why is the CSL_CG_ROOT not set?
And the follow on question, If I set it in the Macros tab, what would I set it to? There is no include folder under "C:\Program Files\Texas Instruments\pspdrivers_01_30_00_06\packages\ti\pspiom\cslr".
And, finally, the curisosity question. is the path "EXT_ROOT__spi_example" a concatenation? How does it know?