Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAPL138
Customer ask the max force can C6748 withstand, need it for mechanical design.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAPL138
Customer ask the max force can C6748 withstand, need it for mechanical design.
Yodan,
Yes, currently it is 0.8mm pitch, will use 0.65mm pitch in new design,
Customer think the data on that post is aging test data. but their concern is during drop test, the enclosure may transform and touch the DSP package, so they need the force can package surface sustain.
OMAPL138/C6748, 361ZCE package option, 0.65mm pitch, 0.4mm ball diameter, SnAgCu solder balls:
@90C ambient temp, Max compressive load to ensure 10 year lifetime: ~155N
OMAPL138/C6748, 361ZWT package option, 0.8mm pitch, 0.5mm ball diameter, SnAgCu solder balls:
@90C ambient temp, Max compressive load to ensure 10 year lifetime: ~330N