Part Number: TMS320C6655
Other Parts Discussed in Thread: ADS8330
Hello TI,
We are looking for TI assistance to help resolve a serial port interface issue we have using TMS320C6655 McBSP port interface to SPI port of ADS8330. We have utilized, and dedicated the SPI interface on C6655 for servicing another critical application module. So we were left with using one of the two McBSP ports on the C6655. TI document “spruhh0.pdf”: KeyStone Architecture Multichannel Buffered Serial Port (McBSP) for C6655 indicates that the McBSP port for this device does not officially support the SPI protocol (Section 2.10 page 62 (2-46)) . We have tried to emulate SPI interface to ADS8330 using a continuous Non-Stop Clock, and using enable/disable sample rate generate FS (frame sync) for Tx/Rx cycles. Our scheme works most of the time on a number circuit packs, but however, we do have some failures we need to eradicate. We can provide further information on the McBSP-SPI emulation software in our design if you aware of any such solution(s).
Thanks