This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: GPMC burst access with DMA

Part Number: AM3352

Hi,

We are having with AM335x GPMC (NAND) burst access with DMA.
It works normal for 4 word, but above 4, the same data is repeated.

This application won't use any OS, its a bare metal application.

Below is the register settings used for 4/8/16 word.

4 word
        GPMC_CONFIG1_3 =  0xF8601201;

8 word
        GPMC_CONFIG1_3 =  0xF8E01201;

16 word
        GPMC_CONFIG1_3 =  0xF9601201;


Result:

4 Word:  Works normal

8 Word:  0 to 3 words are normal, but 4 to 7 words are same as 3rd word

16 Word:  0 to 3 words are normal, but 4 to 15 words are same as 3rd word

3rd word seems to be repeated....

Could you please let me know if there is any settings to be considered
when using GPMC burst access with DMA.

Best Regards
Paddu